Other Parts Discussed in Thread: TEST
Dear TI-Support
In our product we are using an AM571x Sitara processor. We are trying to use the I2C5 Interface from the A15 processor. To initalize the interface I use the method I2C_open(4, NULL) from the TI-RTOS. It will return without an error. Except for I2C_init() no other I2C5 method is called. The A15 crashes than with an exception. I2C1 - 4 are working fine. I can see that the clock is running for I2C5 in the CM_IPU_I2C5_CLKCTRL register. All I2C5 Interrupts are turned off. We are not using the IPUs. If I try to write to the I2C5 register for example SYSTEST than an exception is thrown as well.
Is it still possible to use I2C5 from the A15 instead of the IPU?
Are there any additional initialisation steps needed?
Some additional Informations:
We use the TI-RTOS with pdk 1.0.17
Here is the exception:
Exception occurred in ThreadType_Task.
Task handle: 0xa4030cb0.
Task stack base: 0xa4206d28.
Task stack size: 0x2000.
R0 = 0x4807c000 R8 = 0xa4208a0c
R1 = 0xa4208950 R9 = 0xa4216f00
R2 = 0x801618d8 R10 = 0x00000009
R3 = 0x00000000 R11 = 0xa4208a54
R4 = 0xa42579bc R12 = 0x00000000
R5 = 0xa403231c SP(R13) = 0xa4208a08
R6 = 0xa4032204 LR(R14) = 0x801617dc
R7 = 0x00000000 PC(R15) = 0x801617dc
PSR = 0x600001df
DFSR = 0x00001211 IFSR = 0x00000000
DFAR = 0x00000000 IFAR = 0x00000000
Exception call stack,
0 I2C_open_v1(struct I2C_Config_s *, struct I2C_Params_s *) at I2C_v1.c:807,PC = 0x801617DC FP = 0xA4208A58
When I try to write to the I2C5 register directly the exception happens in the ti_rtos_idle_task.
Thanks for your help.
Kind regards
Marco