Hi,
In our board,the phy chip we use marvell 88e1512。
The phy can be recognized in u-boot, and the phy register can be read and written normally using mii,
but it will fail to obtain the ip automatically using dhcp,
and the ping of the host PC will also fail after manually setting the static IP.
I use an oscilloscope to measure MCU_RGMII1_TXC with a signal of 25Mhz,
and then measure MCU_RGMII1_TD[3:0] with no output.
Please provide the response about this issue.
Best Regards,
jie