Hello Champs,
Customer can run posix timer on PC Ubuntu. But it can run only one time on AM437x board.
What may cause the issue?
Below is the result and code snapshot.
timer1.c
#include <stdio.h> #include <signal.h> #include <time.h> #include <string.h> #include <stdlib.h> #include <unistd.h> void timer_thread(union sigval v) { printf("timer[CLOCK_MONOTONIC] function! %d\n", v.sival_int); } int main() { timer_t timerid; struct sigevent evp; memset(&evp, 0, sizeof(struct sigevent)); //清零初始化 evp.sigev_value.sival_int = 111; //也是标识定时器的,回调函数可以获得 evp.sigev_notify = SIGEV_THREAD; //线程通知的方式,派驻新线程 evp.sigev_notify_function = timer_thread; //线程函数地址 if (timer_create(CLOCK_MONOTONIC, &evp, &timerid) == -1) { perror("fail to timer_create"); exit(-1); } /* 第一次间隔it.it_value这么长,以后每次都是it.it_interval这么长,就是说it.it_value变0的时候会>装载it.it_interval的值 */ struct itimerspec it; it.it_interval.tv_sec = 1; // 回调函数执行频率为1s运行1次 it.it_interval.tv_nsec = 0; it.it_value.tv_sec = 1; // 倒计时3秒开始调用回调函数 it.it_value.tv_nsec = 0; if (timer_settime(timerid, 0, &it, NULL) == -1) { perror("fail to timer_settime"); exit(-1); } //pause(); while (1); return 0; }
Thanks.
Rgds
Shine