Other Parts Discussed in Thread: SYSCONFIG
Sorry,
I import an example application "gpio_input_interrupt_am64x-evm_r5fss0-0_nortos_ti_arm-clang"
but I have a ERROR when running
[Error] Sciclient event config failed!!!
ASSERT: 0.1278s: ../board.c:Sciclient_gpioIrqSet:97: FALSE failed !!!
And I not understanding intrNum = CSLR_R5FSS0_CORE0_INTR_MAIN_GPIOMUX_INTROUTER0_OUTP_8 from?
I have develop a application config MCU_GPIO0_10 (E7) pin as input interrupt but not run
because I can't find interrupt number and parameter config in function "Sciclient_gpioIrqSet"
Can you guide me the parameters to configure the MCU_GPIO0_10 (E7) pin as input interrupt?
Regards,
HieuTa