Other Parts Discussed in Thread: DRA821,
Hi,
This is the related question to the following thread, the customer is considering backplane connections via SGMII directly without PHY.
In this case, they have a concern below.
When the module based on DRA821U which is not yet powered inserts into the backplane, then the some signals put into SGMII port on DRA821 earlier than power via PMIC. It means that the voltage is applied to the SGMII port on DRA821 which not yet powered for a little short time.
Is there any problem on this use case ? Does the SGMII port have a tolerance ? Can DRA821 device and software work fine from booting up ?
Regards,
Hideaki