The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14: PCIe unsupported request

Part Number: 66AK2H14

Hello experts

With a custom board we are running into an issue with PCIe 
(despite not being the first board where we put it in use with this processor)

the setup : 
- one 66AK2H14 as root complex running Linux
- a PCIe switch component
- several 66AK2H14 as endpoints running TI-RTOS
- one FPGA

the Root Complex does its PCIe enumeration and detects all endpoints
Memory Read Write from the Root complex to the FPGA --> works

BUT

memory write from one AK2H14 Endpoint to the FPGA --> no errors reported 
memory READ from one AK2H14 Endpoint to the FPGA --> errors reported

The AK2h14 Endpoint reports a received master abort error
(RX_MST_ABORT bit set in STATUS_COMMAND register, which means it received "a completion with unsupported request completion status"

The PCIe switch port connected to the AK2H14 endpoint sees : 
Correctable Error Detected and Unsupported Request Detected on DEVICE STATUS register
Advisory Non-Fatal Error status on CORRECTABLE ERROR STATUS register

we have checked the obvious (bus master enable etc.) but doesn't see why the transaction is rejected ?

--> any ideas?

Thanks

  • see attached LSPCI info for more details

    lspci_after_read_edited.txt
    ~ # /usr/sbin/lspci -vvv
    = TI SOC ROOT COMPLEX
    00:00.0 Class 0604: Device fffe:eaff (rev 01)
            Control: I/O+ Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Interrupt: pin A routed to IRQ 78
            Region 0: Memory at <ignored> (32-bit, non-prefetchable)
            Bus: primary=00, secondary=01, subordinate=ff, sec-latency=0
            I/O behind bridge: 0000f000-00000fff [empty]
            Memory behind bridge: 50000000-508fffff [size=9M]
            Prefetchable memory behind bridge: fff00000-000fffff [empty]
            Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
                    PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [50] MSI: Enable+ Count=1/1 Maskable- 64bit+
                    Address: 0000000021800054  Data: 0000
            Capabilities: [70] Express (v2) Root Port (Slot-), MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0
                            ExtTag- RBE+
                    DevCtl: CorrErr+ NonFatalErr+ FatalErr+ UnsupReq+
                            RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 5GT/s, Width x2, ASPM L0s, Exit Latency L0s <2us
                            ClockPM- Surprise- LLActRep+ BwNot- ASPMOptComp-
                    LnkCtl: ASPM Disabled; RCB 128 bytes Disabled- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 5GT/s (ok), Width x1 (downgraded)
                            TrErr- Train- SlotClk+ DLActive+ BWMgmt- ABWMgmt-
                    RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna+ CRSVisible-
                    RootCap: CRSVisible-
                    RootSta: PME ReqID 0000, PMEStatus- PMEPending-
                    DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, LTR-, OBFF Not Supported ARIFwd-
                             AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd-
                             AtomicOpsCtl: ReqEn- EgressBlck-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete-, EqualizationPhase1-
                             EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
            Capabilities: [100 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                            MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
                    HeaderLog: 00000000 00000000 00000000 00000000
                    RootCmd: CERptEn+ NFERptEn+ FERptEn+
                    RootSta: CERcvd- MultCERcvd- UERcvd- MultUERcvd-
                             FirstFatal- NonFatalMsg- FatalMsg- IntMsg 0
                    ErrorSrc: ERR_COR: 0000 ERR_FATAL/NONFATAL: 0000
            Kernel driver in use: pcieport
    
    = SWITCH PORT CONNECTED TO TI SOC ROOT COMPLEX 
    01:00.0 Class 0604: Device 12d8:8619
            Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Interrupt: pin ? routed to IRQ 79
            Region 0: Memory at 50800000 (32-bit, non-prefetchable) [size=128K]
            Bus: primary=01, secondary=02, subordinate=11, sec-latency=0
            I/O behind bridge: 0000f000-00000fff [empty]
            Memory behind bridge: 50000000-507fffff [size=8M]
            Prefetchable memory behind bridge: 00000000fff00000-00000000000fffff [empty]
            Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
                    PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0+,D1-,D2-,D3hot+,D3cold+)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [48] MSI: Enable+ Count=1/1 Maskable- 64bit+
                    Address: 0000000021800054  Data: 0001
            Capabilities: [68] Express (v2) Upstream Port, MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0
                            ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ SlotPowerLimit 0.000W
                    DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                            RlxdOrd- ExtTag- PhantFunc- AuxPwr- NoSnoop-
                            MaxPayload 128 bytes, MaxReadReq 128 bytes
                    DevSta: CorrErr+ NonFatalErr- FatalErr- UnsupReq+ AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 5GT/s, Width x1, ASPM L0s, Exit Latency L0s <512ns
                            ClockPM+ Surprise- LLActRep- BwNot- ASPMOptComp-
                    LnkCtl: ASPM Disabled; Disabled- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 5GT/s (ok), Width x1 (ok)
                            TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
                    DevCap2: Completion Timeout: Not Supported, TimeoutDis-, LTR-, OBFF Not Supported
                             AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled
                             AtomicOpsCtl: EgressBlck-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete-, EqualizationPhase1-
                             EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
            Capabilities: [a4] Subsystem: Device 12d8:8619
            Capabilities: [100 v1] Device Serial Number 00-00-00-00-00-00-00-00
            Capabilities: [fb4 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES- TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                            MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
                    HeaderLog: 00000000 00000000 00000000 00000000
            Capabilities: [138 v1] Power Budgeting <?>
            Capabilities: [148 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=4
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=05 MaxTimeSlots=64 RejSnoopTrans-
                            Arb:    Fixed+ WRR32+ WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending- InProgress-
                            Port Arbitration Table <?>
            Capabilities: [270 v1] L1 PM Substates
                    L1SubCap: PCI-PM_L1.2- PCI-PM_L1.1+ ASPM_L1.2- ASPM_L1.1- L1_PM_Substates+
                    L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
    
                    L1SubCtl2:
            Capabilities: [900 v1] Extended Capability ID 0x12
            Kernel driver in use: pcieport
    
    		  
    = SWITCH PORT CONNECTED TO TI SOC ENDPOINT 	
    02:03.0 Class 0604: Device xxxx:xxxx
            Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Interrupt: pin A routed to IRQ 83
            Bus: primary=02, secondary=06, subordinate=06, sec-latency=0
            I/O behind bridge: 0000f000-00000fff [empty]
            Memory behind bridge: 50200000-503fffff [size=2M]
            Prefetchable memory behind bridge: 00000000fff00000-00000000000fffff [empty]
            Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
                    PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0+,D1-,D2-,D3hot+,D3cold+)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [48] MSI: Enable+ Count=1/1 Maskable- 64bit+
                    Address: 0000000021800054  Data: 0005
            Capabilities: [68] Express (v2) Downstream Port (Slot+), MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0
                            ExtTag- RBE+
                    DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                            RlxdOrd- ExtTag- PhantFunc- AuxPwr- NoSnoop-
                            MaxPayload 128 bytes, MaxReadReq 128 bytes
                    DevSta: CorrErr+ NonFatalErr- FatalErr- UnsupReq+ AuxPwr- TransPend-
                    LnkCap: Port #3, Speed 5GT/s, Width x1, ASPM L0s, Exit Latency L0s <512ns
                            ClockPM- Surprise- LLActRep- BwNot+ ASPMOptComp-
                    LnkCtl: ASPM Disabled; Disabled- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s (downgraded), Width x1 (ok)
                            TrErr- Train- SlotClk+ DLActive+ BWMgmt- ABWMgmt-
                    SltCap: AttnBtn+ PwrCtrl+ MRL+ AttnInd+ PwrInd+ HotPlug- Surprise-
                            Slot #0, PowerLimit 25.000W; Interlock- NoCompl-
                    SltCtl: Enable: AttnBtn- PwrFlt- MRL- PresDet- CmdCplt- HPIrq- LinkChg-
                            Control: AttnInd Off, PwrInd On, Power- Interlock-
                    SltSta: Status: AttnBtn- PowerFlt- MRL- CmdCplt- PresDet- Interlock-
                            Changed: MRL- PresDet- LinkState-
                    DevCap2: Completion Timeout: Not Supported, TimeoutDis-, LTR-, OBFF Not Supported ARIFwd+
                             AtomicOpsCap: Routing-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd-
                             AtomicOpsCtl: EgressBlck-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -3.5dB
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
                             EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
            Capabilities: [a4] Subsystem: Device 12d8:8619
            Capabilities: [100 v1] Device Serial Number 00-00-00-00-00-00-00-00
            Capabilities: [fb4 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES- TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                            MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
                    HeaderLog: 00000000 00000000 00000000 00000000
            Capabilities: [148 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=4
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=05 MaxTimeSlots=64 RejSnoopTrans-
                            Arb:    Fixed+ WRR32+ WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending- InProgress-
                            Port Arbitration Table <?>
            Capabilities: [520 v1] Access Control Services
                    ACSCap: SrcValid+ TransBlk+ ReqRedir+ CmpltRedir+ UpstreamFwd+ EgressCtrl+ DirectTrans+
                    ACSCtl: SrcValid- TransBlk- ReqRedir- CmpltRedir- UpstreamFwd- EgressCtrl- DirectTrans-
            Capabilities: [270 v1] L1 PM Substates
                    L1SubCap: PCI-PM_L1.2- PCI-PM_L1.1+ ASPM_L1.2- ASPM_L1.1- L1_PM_Substates+
                    L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
    
                    L1SubCtl2:
            Capabilities: [900 v1] Extended Capability ID 0x12
            Kernel driver in use: pcieport
    
    
    = SWITCH PORT CONNECTED TO FPGA ENDPOINT 		  
    02:0a.0 Class 0604: Device xxxx:xxxx
            Control: I/O- Mem- BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Interrupt: pin A routed to IRQ 89
            Bus: primary=02, secondary=0c, subordinate=0c, sec-latency=0
            I/O behind bridge: 0000f000-00000fff [empty]
            Memory behind bridge: fff00000-000fffff [empty]
            Prefetchable memory behind bridge: 00000000fff00000-00000000000fffff [empty]
            Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
            BridgeCtl: Parity+ SERR- NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
                    PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0+,D1-,D2-,D3hot+,D3cold+)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [48] MSI: Enable+ Count=1/1 Maskable- 64bit+
                    Address: 0000000021800054  Data: 000b
            Capabilities: [68] Express (v2) Downstream Port (Slot+), MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0
                            ExtTag- RBE+
                    DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                            RlxdOrd- ExtTag- PhantFunc- AuxPwr- NoSnoop-
                            MaxPayload 128 bytes, MaxReadReq 128 bytes
                    DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
                    LnkCap: Port #10, Speed 5GT/s, Width x1, ASPM L0s, Exit Latency L0s <512ns
                            ClockPM- Surprise- LLActRep- BwNot+ ASPMOptComp-
                    LnkCtl: ASPM Disabled; Disabled- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s (downgraded), Width x1 (ok)
                            TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
                    SltCap: AttnBtn+ PwrCtrl+ MRL+ AttnInd+ PwrInd+ HotPlug- Surprise-
                            Slot #0, PowerLimit 25.000W; Interlock- NoCompl-
                    SltCtl: Enable: AttnBtn- PwrFlt- MRL- PresDet- CmdCplt- HPIrq- LinkChg-
                            Control: AttnInd Off, PwrInd On, Power- Interlock-
                    SltSta: Status: AttnBtn- PowerFlt- MRL- CmdCplt- PresDet- Interlock-
                            Changed: MRL- PresDet- LinkState-
                    DevCap2: Completion Timeout: Not Supported, TimeoutDis-, LTR-, OBFF Not Supported ARIFwd+
                             AtomicOpsCap: Routing-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd-
                             AtomicOpsCtl: EgressBlck-
                    LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -3.5dB
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
                             EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
            Capabilities: [a4] Subsystem: Device 12d8:8619
            Capabilities: [100 v1] Device Serial Number 00-00-00-00-00-00-00-00
            Capabilities: [fb4 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES- TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                            MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
                    HeaderLog: 00000000 00000000 00000000 00000000
            Capabilities: [148 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=4
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=05 MaxTimeSlots=64 RejSnoopTrans-
                            Arb:    Fixed+ WRR32+ WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending+ InProgress-
                            Port Arbitration Table <?>
            Capabilities: [520 v1] Access Control Services
                    ACSCap: SrcValid+ TransBlk+ ReqRedir+ CmpltRedir+ UpstreamFwd+ EgressCtrl+ DirectTrans+
                    ACSCtl: SrcValid- TransBlk- ReqRedir- CmpltRedir- UpstreamFwd- EgressCtrl- DirectTrans-
            Capabilities: [270 v1] L1 PM Substates
                    L1SubCap: PCI-PM_L1.2- PCI-PM_L1.1+ ASPM_L1.2- ASPM_L1.1- L1_PM_Substates+
                    L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
    
                    L1SubCtl2:
            Capabilities: [900 v1] Extended Capability ID 0x12
            Kernel driver in use: pcieport
    
    
    = TI SOC ENDPOINT 		  
    06:00.0 Class 0480: Device 104c:b008 (rev 01)
            Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort+ >SERR- <PERR- INTx-
            Latency: 0, Cache Line Size: 64 bytes
            Region 0: Memory at 50200000 (32-bit, non-prefetchable) [size=1M]
            Region 1: Memory at 50300000 (32-bit, non-prefetchable) [size=1M]
            Region 2: Memory at <unassigned> (32-bit, prefetchable)
            Region 4: Memory at <unassigned> (32-bit, prefetchable)
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit-
                    Address: 00000000  Data: 0000
    
    					 
    = FPGA ENDPOINT					 
    0a:00.0 Class 0580: Device 10ee:7011
            Subsystem: Device 10ee:0007
            Control: I/O- Mem+ BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Interrupt: pin A routed to IRQ 255
            Region 0: Memory at 50600000 (32-bit, non-prefetchable) [size=1M]
            Region 1: Memory at 50700000 (32-bit, non-prefetchable) [size=64K]
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0+,D1+,D2+,D3hot+,D3cold-)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [48] MSI: Enable- Count=1/1 Maskable- 64bit+
                    Address: 0000000000000000  Data: 0000
            Capabilities: [60] Express (v2) Endpoint, MSI 00
                    DevCap: MaxPayload 512 bytes, PhantFunc 0, Latency L0s <64ns, L1 unlimited
                            ExtTag+ AttnBtn- AttnInd- PwrInd- RBE+ FLReset- SlotPowerLimit 25.000W
                    DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                            RlxdOrd+ ExtTag+ PhantFunc- AuxPwr- NoSnoop+
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 2.5GT/s, Width x1, ASPM L0s, Exit Latency L0s unlimited
                            ClockPM- Surprise- LLActRep- BwNot- ASPMOptComp-
                    LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 2.5GT/s (ok), Width x1 (ok)
                            TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
                    DevCap2: Completion Timeout: Range B, TimeoutDis-, LTR-, OBFF Not Supported
                             AtomicOpsCap: 32bit- 64bit- 128bitCAS-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled
                             AtomicOpsCtl: ReqEn-
                    LnkCtl2: Target Link Speed: 2.5GT/s, EnterCompliance- SpeedDis-
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
                             EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
            Capabilities: [100 v1] Device Serial Number 00-00-00-00-00-00-00-00