1. We are having a device which uses TI's Sitara-am335x processor(Part No: AM3356BZCZD60). We are Currently trying to upgrade to new Micron 8Gb:x8 Flash-model (8SC Part No: MT29F8G08ABACAH4-IT:C)
with page size=4096 Bytes, Block size=256K (256*1024 Bytes).
2. Previously we were using Micron Flash with Part No: MT29F2G08ABAEAH4 with page size=2048 Bytes, Block size=128K (128*1024 Bytes).
3. U-boot compilation throws below error when CONFIG_SYS_NAND_ECCPOS is defined as a 208 Byte array
******Error*******
arm-poky-linux-gnueabi-ld.bfd: u-boot-spl section `.u_boot_list' will not fit in region `.sram'
arm-poky-linux-gnueabi-ld.bfd: region `.sram' overflowed by 400 bytes
****/include/configs/am335x_evm.h MACROs****
#define CONFIG_SYS_NAND_ECCBYTES 26
#define CONFIG_SYS_NAND_ECCPOS { 2, 3, 4, 5, 6, 7, 8, 9, \
10, 11, 12, 13, 14, 15, 16, 17, 18, 19, \
20, 21, 22, 23, 24, 25, 26, 27, 28, 29, \
30, 31, 32, 33, 34, 35, 36, 37, 38, 39, \
40, 41, 42, 43, 44, 45, 46, 47, 48, 49, \
50, 51, 52, 53, 54, 55, 56, 57, 58, 59, \
60, 61, 62, 63, 64, 65, 66, 67, 68, 69, \
70, 71, 72, 73, 74, 75, 76, 77, 78, 79, \
80, 81, 82, 83, 84, 85, 86, 87, 88, 89, \
90, 91, 92, 93, 94, 95, 96, 97, 98, 99, \
100, 101, 102, 103, 104, 105, 106, 107, 108, 109, \
110, 111, 112, 113, 114, 115, 116, 117, 118, 119, \
120, 121, 122, 123, 124, 125, 126, 127, 128, 129, \
130, 131, 132, 133, 134, 135, 136, 137, 138, 139, \
140, 141, 142, 143, 144, 145, 146, 147, 148, 149, \
150, 151, 152, 153, 154, 155, 156, 157, 158, 159, \
160, 161, 162, 163, 164, 165, 166, 167, 168, 169, \
170, 171, 172, 173, 174, 175, 176, 177, 178, 179, \
180, 181, 182, 183, 184, 185, 186, 187, 188, 189, \
190, 191, 192, 193, 194, 195, 196, 197, 198, 199, \
200, 201, 202, 203, 204, 205, 206, 207, 208, 209, \
}
******When MACROs defined like below compilation is successful******
#define CONFIG_SYS_NAND_ECCBYTES 14
#define CONFIG_SYS_NAND_ECCPOS { 2, 3, 4, 5, 6, 7, 8, 9, \
10, 11, 12, 13, 14, 15, 16, 17, \
18, 19, 20, 21, 22, 23, 24, 25, \
26, 27, 28, 29, 30, 31, 32, 33, \
34, 35, 36, 37, 38, 39, 40, 41, \
42, 43, 44, 45, 46, 47, 48, 49, \
50, 51, 52, 53, 54, 55, 56, 57, }
******Other definitions in am335x_evm.h******
#define CONFIG_SYS_NAND_PAGE_SIZE 4096
#define CONFIG_SYS_NAND_OOBSIZE 224
#define CONFIG_SYS_NAND_BLOCK_SIZE (256*1024)
#define CONFIG_NAND_OMAP_ECCSCHEME OMAP_ECC_BCH16_CODE_HW
Please advise what should be the correct definitions for above MACROs.