This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA77P: DRA77P: fastboot 0 fails when using USB3.0 connection (2)

Part Number: DRA77P


Hi

As the original question is closed without any comments, I ask the same question again:



We're having issues with this setup:

- DRA77P EVM board,

- USB3.0 A to microB cable

- PC with USB3.0 connectors

- mini-USB to USB connector.

When we stop u-boot and enter fastboot 0, the USB3.0 is reconiced by Windows but with problems (but descriptor). This issue is solved if we use a USB2.0 cable connected to the USB3.0 cable.

My question is: can't we connect the EVM to a PCB via a 3.0 connection when using fastboot 0? Why?

Regards,