Hi Everyone,
when trying to build meta-ti-extras/recipes-ti/devtools/ti-cg-xml_2.61.00.bb the recipe fails on my build machine during the do_install() step. I figured out, that the Linux - cgxml-2.61.00-linux-installer.run always fails to execute with errno 127 which leads to an error in the do_install() step because there are not files unpacked which could be installed.
The build host is running ubuntu 20.04. Because the cgxml installer is a 32 bit binary, I have installed libc6-i386 and so /lib/ld-linux.so.2 is correctly linked to /lib32/ld-linux.so.2.
Does anyone have an idea how to get the cgxml installer correctly running on my machine?
Thanks,
Marco