Hello community ,
I am trying to execute the "Face Detection Demo" for LCDKC6748 but unable to get the output.I have already installed the related software package and IDE like bios_c6sdk_02_00_00_00_setupwin32 and ccs_setup_5.1.0.09000 which was available in SYS/BIOS (SD Card ). I have successfully imported and compiled the project into my workspace.Once the code is compiled I am able to see the .out file is generated.After debugging the code I am unable to get the output.
Whether I need to use any specific camera and/or cable ?
I am using the Analog CCD camera and AV cable and I also tried with Y-Cable.
Thank You.