I am working with CCS v11.2 and MCSDK v2.1.2.6 connected to a TMDXEVM6678LXE EVM board. I have been able to build and run the HUA demo example as well as the Multicore LED PLAY DDR3 example. So far everything is working very well. I can build, run and even single-step and debug these applications. Could you please recommend a starting point for the following use case:
- One core (say Core0) running UDP/IP/ETH to an external application that can share messages/data with a second core (say Core1).
Thank you very much,
Bill