This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6657: TMDSEVM6657 - HelloWorld project of NDK

Part Number: TMDSEVM6657


Hi. I'm Han who is totally newbie at TI DSP.

I wanted to run the example project of NDK. So, I downloaded CCS and SDK.

This is the thing what I downloaded.

   1. Code composer studio 9.3.0.00012

   2. ti-processor-sdk-rtos-c665x-evm-06.03.00.106-Windows-x86-Install.exe

I built SDK, PDK and I could get the example project of NDK(NIMU_emacExample_EVMC6657C66BiosExampleProject).

I followed the steps of SPRAC57, section 4.

(I'm not sure of GEL file. GEL file that I use is "C:/ti/ccs930/ccs/ccs_base/emulation/boards/evmc6657l/gel/evmc6657l.gel".)

Below is the result of running example code. (STATIC IP)

and I ran the helloWorld.exe in the ndk_3_61_01_01\packages\ti\ndk\winapps with EVK IP.

I thought I can see the HelloWorld phrase but I can't.

Below is the result.

and I thought I can ping test to EVK but it not works. The text what I saw is "Destination host unreachable".

Plz tell me what should I do to see the result.

If my info is not enough to understand, just let me know.

** the thing I touched in the helloWorld_c6657.c is just if (0) <-> if (1) for DHCP or STATIC IP.