How to run NIMU EMAC examples from TI-RTOS SDK on K2H devices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
To run the NIMU EMAC example for K2H devices make sure the pre-requisites are present.
Now Import the CCS project into CCS and go on

//---------------------------------------------------------------------------
// Local IP and gateway IP can be modified to our requirement
//
char *HostName = "tidsp";
char *LocalIPAddr = "192.168.1.4";
char *LocalIPMask = "255.255.255.0"; // Not used when using DHCP
char *GatewayIP = "192.168.1.1"; // Not used when using DHCP
char *DomainName = "demo.net"; // Not used when using DHCP
char *DNSServer = "0.0.0.0"; // Used when set to anything but zero
//
// Main Thread
//
int StackTest()
{
...
// If the IP address is specified, manually configure IP and Gateway
#if defined(_SCBP6618X_) || defined (DEVICE_C6678) || defined(_EVMTCI6614_) || defined(DEVICE_K2H) || defined(DEVICE_K2K) || defined(DEVICE_K2L) || defined(DEVICE_K2E)
/* SCBP6618x, EVMTCI6614, EVMK2H, EVMK2K always uses DHCP */
if (1) // set it as 1 for Manual IP configuration
{
//Manual IP configuration code
}
else
{
//DHCP IP configuration code
}
...
}



//
// Main Thread
//
int StackTest()
{
...
// If the IP address is specified, manually configure IP and Gateway
#if defined(_SCBP6618X_) || defined (DEVICE_C6678) || defined(_EVMTCI6614_) || defined(DEVICE_K2H) || defined(DEVICE_K2K) || defined(DEVICE_K2L) || defined(DEVICE_K2E)
/* SCBP6618x, EVMTCI6614, EVMK2H, EVMK2K always uses DHCP */
if (0) // set it as 0 for DHCP IP configuration
{
//Manual IP configuration code
}
else
{
//DHCP IP configuration code
}
...
}


Output for DHCP in the ARM core
Thanks & Regards,
Rajarajan U