This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: Not able to boot from SPI and reboot also not working. Needed SPI NOR Uboot & kernel support for chip (MX25L25735FZ2I-10G)

Part Number: AM5748


Hi All,

We are developing custom board using AM5748 SOC. we were able to read, write and erase from spi nor

( MX25L25735FZ2I-10G ) on uboot and kernel. but board is booting from SD card only not from SPI flash.

if we boot from the SDcard not able to reboot and reset.

Uboot version:- u-boot-2018.01 part of the sdk

Kernel version:- 4.14.40

Please let us know something about to change on this source. 

Thanks in advance,

Uthayakumar RH