Hi Team,
I want to use TMDSICE3359 as an EtherCAT board for my project. For this I have done the following steps:
- Created bootable SD Card and copied both MLO (from RTOS SDK ver 6.3.106) and APP(from pru_icss_ethercat_slave_prebuilt_01.00.10.00).
- Erased SPI flash on the EVm.
- Plugged in the SD card and powered up the board.
- I reset the board and observed led pattern as desired.
- Again I reset the board ,while running minicom serial terminal open, following is the capture from minicom
My questions are,
- why my minicom is showing status offline while the board is still connected and LED are showing the expected pattern?
- As a start I am using SOEM master simple test to get the details of the slave. But the program fails to identify the ICE board. Why this happens?[following is the output for SOEM master simple test program].
- is this prebuilt app running continuously on the board or is it a one time process?
Regards,
Vineeth