Hi TI Team,
We have downloaded the AM62x Linux SDK by following the instructions from https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/08_03_00_19/exports/docs/linux/Overview_Building_the_SDK.html#overview-building-the-sdk and had given the following commands for compilation.
1. git clone git.ti.com/.../oe-layersetup.git tisdk
2. cd tisdk
3. ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-08.03.00.19-config.txt
4. cd build
5. . conf/setenv
6. export TOOLCHAIN_PATH_ARMV7=$HOME/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf
7. export TOOLCHAIN_PATH_ARMV8=$HOME/gcc-arm-9.2-2019.12-x86_64-aarch64
8. MACHINE=am62xx-evm bitbake meta-toolchain-arago-tisdk
When we are compiling, we are facing the following no such file/directory issue but when we are trying to find those files, the files are already present in the directory.
Please help in resolving the issue.
"cp: cannot stat '/home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/{libstdc++.*,libgcc_s.*,libsupc++.*}': No such file or directory"
"cp: cannot stat '/home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/{libstdc++.*,libgcc_s.*,libsupc++.*}': No such file or directory"
Complete log file is attached (compilation_error.txt)
ranjithkv@tisdk:~/tisdk/build$ MACHINE=am62xx-evm bitbake meta-toolchain-arago-tisdk NOTE: Started PRServer with DBfile: /home/ranjithkv/tisdk/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 42923, PID: 8628 Loading cache: 100% |#######################################################################################################################################################################| Time: 0:00:01 Loaded 8266 entries from dependency cache. NOTE: Resolving any missing task queue dependencies NOTE: Resolving any missing task queue dependencies NOTE: Resolving any missing task queue dependencies NOTE: Resolving any missing task queue dependencies Build Configuration: BB_VERSION = "1.46.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-18.04" TARGET_SYS = "aarch64-linux" MACHINE = "am62xx-evm" DISTRO = "arago" DISTRO_VERSION = "2021.09" TUNE_FEATURES = "aarch64" TARGET_FPU = "" meta-processor-sdk = "HEAD:b39d454b1622e53a23a08c5470ba6de2162264df" meta-arago-distro meta-arago-extras = "HEAD:aa5fd0df1e0392703f7929c407ee1caf0f40b5aa" meta-qt5 = "HEAD:5ef3a0ffd3324937252790266e2b2e64d33ef34f" meta-virtualization = "HEAD:f6b88c1d2f515ffac90457c0d649d6c805fff736" meta-networking meta-python meta-oe meta-gnome meta-filesystems = "HEAD:8ff12bfffcf0840d5518788a53d88d708ad3aae0" meta-ti = "HEAD:e99d9aa3fc41fa3a91d68ad9e654d40bfb6e0967" meta-arm meta-arm-toolchain = "HEAD:c4f04f3fb66f8f4365b08b553af8206372e90a63" meta = "HEAD:48ce924dc82aa959fb897ec36873db7dc3813b71" Build Configuration: BB_VERSION = "1.46.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-18.04" TARGET_SYS = "arm-linux-gnueabi" MACHINE = "am62xx-evm-k3r5" DISTRO = "arago" DISTRO_VERSION = "2021.09" TUNE_FEATURES = "arm armv7a vfp thumb callconvention-hard" TARGET_FPU = "hard" meta-processor-sdk = "HEAD:b39d454b1622e53a23a08c5470ba6de2162264df" meta-arago-distro meta-arago-extras = "HEAD:aa5fd0df1e0392703f7929c407ee1caf0f40b5aa" meta-qt5 = "HEAD:5ef3a0ffd3324937252790266e2b2e64d33ef34f" meta-virtualization = "HEAD:f6b88c1d2f515ffac90457c0d649d6c805fff736" meta-networking meta-python meta-oe meta-gnome meta-filesystems = "HEAD:8ff12bfffcf0840d5518788a53d88d708ad3aae0" meta-ti = "HEAD:e99d9aa3fc41fa3a91d68ad9e654d40bfb6e0967" meta-arm meta-arm-toolchain = "HEAD:c4f04f3fb66f8f4365b08b553af8206372e90a63" meta = "HEAD:48ce924dc82aa959fb897ec36873db7dc3813b71" Initialising tasks: 100% |##################################################################################################################################################################| Time: 0:00:04 Sstate summary: Wanted 1623 Found 0 Missed 1623 Current 440 (0% match, 21% complete) NOTE: Executing Tasks ERROR: external-arm-sdk-toolchain-armv7a-1.0-r9 do_install: Execution of '/home/ranjithkv/tisdk/build/arago-tmp-external-arm-glibc/work/x86_64-nativesdk-arago-linux/external-arm-sdk-toolchain-armv7a/1.0-r9/temp/run.do_install.8850' failed with exit code 1 ERROR: Logfile of failure stored in: /home/ranjithkv/tisdk/build/arago-tmp-external-arm-glibc/work/x86_64-nativesdk-arago-linux/external-arm-sdk-toolchain-armv7a/1.0-r9/temp/log.do_install.8850 Log data follows: | DEBUG: Executing python function extend_recipe_sysroot | NOTE: Direct dependencies are ['virtual:native:/home/ranjithkv/tisdk/sources/oe-core/meta/recipes-devtools/chrpath/chrpath_0.16.bb:do_populate_sysroot', '/home/ranjithkv/tisdk/sources/oe-core/meta/recipes-devtools/quilt/quilt-native_0.66.bb:do_populate_sysroot', 'virtual:native:/home/ranjithkv/tisdk/sources/oe-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot'] | NOTE: Installed into sysroot: [] | NOTE: Skipping as already exists in sysroot: ['chrpath-native', 'quilt-native', 'pseudo-native', 'autoconf-native', 'libtool-native', 'gnu-config-native', 'automake-native', 'texinfo-dummy-native', 'm4-native'] | DEBUG: Python function extend_recipe_sysroot finished | DEBUG: Executing shell function do_install | cp: cannot stat '/home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/{libstdc++.*,libgcc_s.*,libsupc++.*}': No such file or directory | WARNING: exit code 1 from a shell command. | ERROR: Execution of '/home/ranjithkv/tisdk/build/arago-tmp-external-arm-glibc/work/x86_64-nativesdk-arago-linux/external-arm-sdk-toolchain-armv7a/1.0-r9/temp/run.do_install.8850' failed with exit code 1 ERROR: Task (/home/ranjithkv/tisdk/sources/meta-arago/meta-arago-distro/recipes-core/meta/external-arm-secondary-sdk-toolchain.bb:do_install) failed with exit code '1' ERROR: external-arm-sdk-toolchain-aarch64-1.0-r9 do_install: Execution of '/home/ranjithkv/tisdk/build/arago-tmp-external-arm-glibc/work/x86_64-nativesdk-arago-linux/external-arm-sdk-toolchain-aarch64/1.0-r9/temp/run.do_install.8851' failed with exit code 1 ERROR: Logfile of failure stored in: /home/ranjithkv/tisdk/build/arago-tmp-external-arm-glibc/work/x86_64-nativesdk-arago-linux/external-arm-sdk-toolchain-aarch64/1.0-r9/temp/log.do_install.8851 Log data follows: | DEBUG: Executing python function extend_recipe_sysroot | NOTE: Direct dependencies are ['virtual:native:/home/ranjithkv/tisdk/sources/oe-core/meta/recipes-devtools/chrpath/chrpath_0.16.bb:do_populate_sysroot', '/home/ranjithkv/tisdk/sources/oe-core/meta/recipes-devtools/quilt/quilt-native_0.66.bb:do_populate_sysroot', 'virtual:native:/home/ranjithkv/tisdk/sources/oe-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot'] | NOTE: Installed into sysroot: [] | NOTE: Skipping as already exists in sysroot: ['chrpath-native', 'quilt-native', 'pseudo-native', 'autoconf-native', 'libtool-native', 'gnu-config-native', 'automake-native', 'texinfo-dummy-native', 'm4-native'] | DEBUG: Python function extend_recipe_sysroot finished | DEBUG: Executing shell function do_install | cp: cannot stat '/home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/{libstdc++.*,libgcc_s.*,libsupc++.*}': No such file or directory | WARNING: exit code 1 from a shell command. | ERROR: Execution of '/home/ranjithkv/tisdk/build/arago-tmp-external-arm-glibc/work/x86_64-nativesdk-arago-linux/external-arm-sdk-toolchain-aarch64/1.0-r9/temp/run.do_install.8851' failed with exit code 1 ERROR: Task (/home/ranjithkv/tisdk/sources/meta-arago/meta-arago-extras/recipes-core/meta/external-arm-sdk-toolchain.bb:do_install) failed with exit code '1' Second Keyboard Interrupt, stopping... Summary: 2 tasks failed: /home/ranjithkv/tisdk/sources/meta-arago/meta-arago-distro/recipes-core/meta/external-arm-secondary-sdk-toolchain.bb:do_install /home/ranjithkv/tisdk/sources/meta-arago/meta-arago-extras/recipes-core/meta/external-arm-sdk-toolchain.bb:do_install Summary: There were 2 ERROR messages shown, returning a non-zero exit code. ranjithkv@tisdk:~/tisdk/build$ ls /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/{libstdc++.*,libgcc_s.*,libsupc++.*} /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libgcc_s.so /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libgcc_s.so.1 /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libstdc++.a /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libstdc++.so /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libstdc++.so.6 /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libstdc++.so.6.0.28 /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libstdc++.so.6.0.28-gdb.py /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/aarch64-none-linux-gnu/lib64/libsupc++.a ranjithkv@tisdk:~/tisdk/build$ ls /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/{libstdc++.*,libgcc_s.*,libsupc++.*} /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libgcc_s.so /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libgcc_s.so.1 /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libstdc++.a /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libstdc++.so /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libstdc++.so.6 /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libstdc++.so.6.0.28 /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libstdc++.so.6.0.28-gdb.py /home/ranjithkv/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/arm-none-linux-gnueabihf/lib/libsupc++.a