Other Parts Discussed in Thread: UNIFLASH
Hi All,
System Specification:
1. Processor : AM3354
2. SDK : Bare-metal
3. Programming interface : JTAG
4. External interfaces : UART, Ethernet
5. eMMC : Yes connected with MMC0. Size 4GB, Part number : MTFC4GLWDM-4M AAT A
6. RAM : External RAM DDR3, size 512Mb, part : MT41K512M8DA-107
7. SD card support : No SD card slot.
Requirement:
1. Application image need to be flashed into the eMMC through UART/Ethernet.
2. Application image need to be booted form eMMC after power-ON.
Queries:
1. How to flash the application image into the eMMC without SD card, through UART/Ethernet only?
2. What are SW tools required for the flashing?
3. What are the boot configuration required?