Hello
We have created a board design using LPDDR4 and attempting to get signs of life out of the unit.
Using the SDK and the AM65x_DRA80xM_EMIF_Tool_2.02.xlsm spreadsheet we have entered all the relevant timing information to generate the k3-am654-base-board-lpddr4-1600MTs.dtsi
Uboot has been modified to use the newly generated k3-am654-base-board-lpddr4-1600MTs.dtsi
Built using the SDK Makefile with
# make u-boot
# make sysfw-image
Outputted files of:
sysfw-am65x-evm.itb
tiboot3.bin
tispl.bin
uEnv.txt
Written to bootable SD card and used to boot the board.
We can see some clock activity to access the SD card but then it stops. This happens for both the release image suppled by Ti and our built image.
We understand that the AM65x EVM is DDR4 based and our change is LPDDR4 but need to find a way to ensure the DRAM configuration changes are being applied to the setup with the r5 processor.
Is there currently any known working configuration or image for LPDDR4 and AM65x ?
Thank you
Marc