Hi,
we would like to implement 1.8V low voltage signaling (LVS) interface for SD card at MMC0 and also use this SD Card interface as a bootable medium during the board bringing .
Also we would like to use it in MMC/SD 4-bit mode.
Following pins are mapped to the VDDSHV1 power bank:
D1: MMC0_CLK
D2: MMC_CMD
C1: MMC_DAT0
C2: MMC_DAT1
B2: MMC_DAT2
B1: MMC_DAT3
Is it enough just to switch the VDDHV1 bank to 1.8 V power rail in order to support 1.8V low voltage signaling (LVS) interface SD Cards?
According to the data sheet, chapter 5.12.17.1 MMC Electrical Data and Timing, AM4376 should support 1.8V signaling for SD cards, correct?
What should we take care about linux image in order to support 1.8V signaling SD cards?
Up to now we have been using VDDHV1 bank at 3.3V.
The SD card we would like to use it: i300 microSDXC Card (mouser.at)
Regards