I see that the MPM daemon can run a script of mpmcl commands upon boot and the location of that script is pointed to by the 3rd line of mpm_config.json file. In the SDK distribution the line includes an underscore to cmdfile which causes it to be ignored.
"_cmdfile": "/etc/mpm/slave_cmds.txt"
As noted in the related post, the underscore needs to be removed to allow CJSON to be able to parse that line. My question is: Where is the source for the mpm_config.json file so that I can edit the source content so it will be generated correctly during the build?
I see it in the MPM package under scripts folder but I don't see an install target that would install that to the target's rootfs during the build.
Please advise.
Thanks