Hello,
I will install and run vision_apps demos on SK-TDA4VM, I have installed vision_apps according to the chapter of SDK Development flow of the user guide, both the SDK version of RTOS and SK-TDA4VM is v8.01,
I test the demo as the following command:
root@j7-evm:/opt/vision_apps# source ./vision_apps_init.sh
root@j7-evm:/opt/vision_apps# ./run_app_tidl.sh
the debug information as following:
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
3829.988175 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
3829.988241 s: VX_ZONE_INIT:Enabled
3829.988266 s: VX_ZONE_ERROR:Enabled
3829.988284 s: VX_ZONE_WARNING:Enabled
3829.988778 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
3829.988997 s: VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for HOST !!!
It seems that the action of run_app_tidl was not complete, would you please tell me how to do, thanks a lot!
B.R
Donghui Zhu