Other Parts Discussed in Thread: TPS65910
Hi,
My customer are using AM3356 and TPS65910A31A1 as a power supply of AM3356.
And they are having some issue on the power line VDD2(PMIC) - VDD_CORE(AM3356).
We don't know the cause yet, but the current of VDD_CORE fluctuates from 0mA to about 600mA in 10us period.
(0mA -> 600mA -> 0mA -> 600mA -> -----)
In the datasheet of AM335x, it's written as that VDD_CORE current range is 400mA(maximum).
Will VDD_CORE ever exceed this 400mA?
best regards,
g.f.