Other Parts Discussed in Thread: AM5728
Hi,
I tried to build SDK Linux for use with AM572x IDK. But i got error as given below.
I followed the procedures given in Processor SDK Linux for AM57X 08_02_01_00
Please help to solve this error.
=================================
Building the Linux Kernel
=================================
.
.
.
/media/Linux-PC/BCU/AM572x-SDK-08-00/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-none-linux-gnueabihf/9.2.1/plugin/include/system.h:687:10: fatal error: gmp.h: No such file or directory
#include <gmp.h>
^~~~~~~
compilation terminated.
scripts/gcc-plugins/Makefile:47: recipe for target 'scripts/gcc-plugins/arm_ssp_per_task_plugin.so' failed
make[3]: *** [scripts/gcc-plugins/arm_ssp_per_task_plugin.so] Error 1
scripts/Makefile.build:497: recipe for target 'scripts/gcc-plugins' failed
make[2]: *** [scripts/gcc-plugins] Error 2
Makefile:1199: recipe for target 'scripts' failed
make[1]: *** [scripts] Error 2
make[1]: Leaving directory '/media/Linux-PC/BCU/AM572x-SDK-08-00/board-support/linux-5.10.100+gitAUTOINC+7a7a3af903-g7a7a3af903'
Makefile:10: recipe for target 'linux' failed
make: *** [linux] Error 2