Hi Team,
In asynchronous access to the external memory area (CE2) via EMIFA, when the access (CE2 read) from the CPU was continuously executed, the low pulse interval of CE2 was about 250 ns which was slower than expected.
The settings are as follows.
SYSTEM_CLK1: 336 MHz
SYSTEM_CLK3: 84 MHz
EMIFA.CE2CFG=0x80000001
Reading the Datasheet Table 6-22. EMIFA Asynchronous Memory Switching Characteristics
I understood that the interval between accesses is what was defined by No.1 Turn around time(1 CLOCK of SYSCLK3 ± 3 ns).
I compiled in debug mode, but does it change by compilation modes?
Does the EMIFA asynchronous serial access automatically insert an interval of about 250 ns?
Is DMA transfer a similar operation?
Beat Regards,
Tom Liu