This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No EMAC interrupts generated on the 6486 or 6472 reference board.



Hi,

I am trying to modify the Helloworld_evm6472 project that came with MCSDK1.0 to work on the custom reference board with a C6486 on it. I removed the platform specific EVM inits.

Here we do not have a PHY. But the FPGA sends ethernet frames to the DSP at a fixed MAC address. I have configured the PLLs correctly and set the EMAC receive filter, MAC address correctly I think. So, EMAC0 - RXGOODFRAMES register increments. I verified that the interrupt initialization is also okay.

But, I do not see any interrupts generated i.e I am never able to hit the breakpoint in emac_rx_packet() in the EMAC driver.

Can anyone tell me why no interrupts are generated?

 

Thanks.,

Arun