This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: No image shows on GUI after building SDK

Genius 13655 points
Part Number: AM3358
Other Parts Discussed in Thread: AM3352, TPS65910

Hello Champs,

HW: am335x starter kit

SDK: ti-processor-sdk-linux-am335x-evm-08.02.00.24

Ubuntu 18.04

Customer built the SDK and got a tisdk-default-image according to 1.2. Building the SDK — Processor SDK Linux for AM335X Documentation , but after it booted up, it stuck at please wait....., the GUI shows nothing but black. However, he can boot the default-image:https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-1BUptXj3op/07.03.00.005/am335x-evm-linux-tisdk-default-image-07.03.00.005.wic.xz, the GUI can show correctly. 

Because there is something wrong when executing bitbake, he modified below code:

${home}=/home/fffengzia/ti-processor-sdk-linux-am335x-evm-08.02.00.24/tisdk
=========================================================================
| PROBLEM SCRIPTION: |
=========================================================================

| ${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/build/Bootstrap.cmk/cmake:
/usr/lib/x86_64-linux-gnu/libstdc++.so.6: version `GLIBCXX_3.4.26' not found
(required by ${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/build/Bootstrap.cmk/cmake)

| ---------------------------------------------
| Error when bootstrapping CMake:
| Problem while running initial CMake
| ---------------------------------------------

| WARNING:
${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/temp/run.do_configure.13063:1 exit 11
from '${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/cmake-3.16.5/configure
--verbose --prefix=${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/recipe-sysroot-native/usr
--parallel=3
--
-DCMAKE_LIBRARY_PATH=${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/recipe-sysroot-native/usr/lib
-DBUILD_CursesDialog=1
-DCMAKE_USE_SYSTEM_LIBRARIES=1
-DCMAKE_USE_SYSTEM_LIBRARY_JSONCPP=0
-DCMAKE_USE_SYSTEM_LIBRARY_LIBARCHIVE=0
-DCMAKE_USE_SYSTEM_LIBRARY_LIBUV=0
-DCMAKE_USE_SYSTEM_LIBRARY_LIBRHASH=0
-DENABLE_ACL=0
-DHAVE_ACL_LIBACL_H=0
-DHAVE_SYS_ACL_H=0'

| ERROR:
Execution of
'${home}/build/arago-tmp-external-arm-glibc/work/x86_64-linux/cmake-native/3.16.5-r0/temp/run.do_configure.13063' failed with exit code 11

+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Deal:
update libstdc++ or other packages
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++


=========================================================================
| PROBLEM SCRIPTION: |
=========================================================================
ERROR:
mobile-broadband-provider-info-1_20201225-r0 do_fetch:
Fetcher failure:
Unable to find revision 90f3fe28aa25135b7e4a54a7816388913bfd4a2a in branch master even from upstream

ERROR:
mobile-broadband-provider-info-1_20201225-r0 do_fetch:
Bitbake Fetcher Error:
FetchError
('Unable to fetch URL from any source.', 'git://gitlab.gnome.org/GNOME/mobile-broadband-provider-info.git;protocol=https;branch=master')

ERROR:
Logfile of failure stored in:
${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/mobile-broadband-provider-info/1_20201225-r0/temp/log.do_fetch.40614

ERROR:
Task
(${home}/sources/oe-core/meta/recipes-connectivity/mobile-broadband-provider-info/mobile-broadband-provider-info_git.bb:do_fetch)
failed with exit code '1'

++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
${home}/sources/oe-core/meta/recipes-connectivity/mobile-broadband-provider-info/mobile-broadband-provider-info_git.bb
Deal: Change the SRCREV in .bb from "90f3fe28aa25135b7e4a54a7816388913bfd4a2a" into "fe19892a8168bf19d81e3bc4ee319bf7f9f058f5";
branch=master into branch=main;
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++


=========================================================================
| PROBLEM SCRIPTION: |
=========================================================================
ERROR: linux-ti-staging-5.10.65+gitAUTOINC+dcc6bedb2c-r22b.arago5 do_package: Error executing a python function in exec_func_python() autogenerated:

The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_func_python() autogenerated', lineno: 2, function: <module>
0001:
*** 0002:do_package(d)
0003:
File: '${home}/sources/oe-core/meta/classes/package.bbclass', lineno: 2315, function: do_package
2311:
2312: cpath = oe.cachedpath.CachedPath()
2313:
2314: for f in (d.getVar('PACKAGESPLITFUNCS') or '').split():
*** 2315: bb.build.exec_func(f, d)
2316:
2317: ###########################################################################
2318: # Process PKGDEST
2319: ###########################################################################
File: '${home}/sources/bitbake/lib/bb/build.py', lineno: 254, function: exec_func
0250: with bb.utils.fileslocked(lockfiles):
0251: if ispython:
0252: exec_func_python(func, d, runfile, cwd=adir)
0253: else:
*** 0254: exec_func_shell(func, d, runfile, cwd=adir)
0255:
0256: try:
0257: curcwd = os.getcwd()
0258: except:
File: '${home}/sources/bitbake/lib/bb/build.py', lineno: 455, function: exec_func_shell
0451: with open(fifopath, 'r+b', buffering=0) as fifo:
0452: try:
0453: bb.debug(2, "Executing shell function %s" % func)
0454: with open(os.devnull, 'r+') as stdin, logfile:
*** 0455: bb.process.run(cmd, shell=False, stdin=stdin, log=logfile, extrafiles=[(fifo,readfifo)])
0456: finally:
0457: os.unlink(fifopath)
0458:
0459: bb.debug(2, "Shell function %s finished" % func)
File: '${home}/sources/bitbake/lib/bb/process.py', lineno: 184, function: run
0180:
0181: if pipe.returncode != 0:
0182: if log:
0183: # Don't duplicate the output in the exception if logging it
*** 0184: raise ExecutionError(cmd, pipe.returncode, None, None)
0185: raise ExecutionError(cmd, pipe.returncode, stdout, stderr)
0186: return stdout, stderr
Exception:
bb.process.ExecutionError:
Execution of '${home}/build/arago-tmp-external-arm-glibc/work/am335x_evm-linux-gnueabi/linux-ti-staging/5.10.65+gitAUTOINC+dcc6bedb2c-r22b.arago5/temp/run.populate_srcipk_package.37953' failed with exit code 1

ERROR:
Logfile of failure stored in:
${home}/build/arago-tmp-external-arm-glibc/work/am335x_evm-linux-gnueabi/linux-ti-staging/5.10.65+gitAUTOINC+dcc6bedb2c-r22b.arago5/temp/log.do_package.37953

ERROR: Task (${home}/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_5.10.bb:do_package) failed with exit code '1'


+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Deal:
step1:
in file: ${home}/sources/meta-ti/recipes-kernel/linux/setup-defconfig.inc:
annotate:
3 def get_git_revision(p):
4 import subprocess
5
6 try:
7 return subprocess.Popen("git rev-parse HEAD 2>/dev/null ", cwd=p, shell=True, stdout=subprocess.PIPE, universal_newlines=True).communicate()[0].rstrip()
8 except OSError:
9 return None

change:
11 KERNEL_LOCALVERSION = "-g${@get_git_revision('${S}').__str__()[:10]}"
into:
KERNEL_LOCALVERSION = "-g${@d.getVar('SRCPV', True).split('+')[1]}"

step2:
in file: ${home}/sources/meta-ti/recipes-bsp/u-boot/u-boot-ti.inc:
annotate:
3 def get_git_revision(p):
4 import subprocess
5
6 try:
7 return subprocess.Popen("git rev-parse HEAD 2>/dev/null ", cwd=p, shell=True, stdout=subprocess.PIPE, universal_newlines=True).communicate()[0].rstrip()
8 except OSError:
9 return None

change:
UBOOT_LOCALVERSION = "-g${@get_git_revision('${S}').__str__()[:10]}"
into:
UBOOT_LOCALVERSION = "-g${@d.getVar("SRCREV", False).__str__()[:10]}"

NOTE:
The change in step2 maybe different, for more details please go to:
e2e.ti.com/.../faq-yocto-building-the-linux-sdk-results-in-do_package-failures-for-linux-kernel-and-u-boot
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

=========================================================================
| PROBLEM SCRIPTION: |
=========================================================================
| /home/fffengzia/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/bin/../lib/gcc/arm-none-linux-gnueabihf/9.2.1/../../../../arm-none-linux-gnueabihf/bin/ld:
.obj/tst_qmetatype.o:
(.debug_info+0x52a5d9): undefined reference to `.LVUS46803'

| collect2: error: ld returned 1 exit status
| Makefile:108: recipe for target 'tst_qmetatype' failed
i make[5]: *** [tst_qmetatype] Error 1
| make[5]: Leaving directory
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/build/tests/auto/corelib/kernel/qmetatype'
| Makefile:316: recipe for target 'sub-qmetatype-make_first' failed
| make[4]: *** [sub-qmetatype-make_first] Error 2
| make[4]: Leaving directory
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/build/tests/auto/corelib/kernel'
| Makefile:59: recipe for target 'sub-kernel-make_first' failed
| make[3]: *** [sub-kernel-make_first] Error 2
| make[3]: Leaving directory
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/build/tests/auto/corelib'
| Makefile:57: recipe for target 'sub-corelib-make_first' failed
| make[2]: *** [sub-corelib-make_first] Error 2
| make[2]: Leaving directory
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/build/tests/auto'
| Makefile:47: recipe for target 'sub-auto-make_first' failed
| make[1]: *** [sub-auto-make_first] Error 2
| make[1]: Leaving directory
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/build/tests'

| Makefile:100: recipe for target 'sub-tests-make_first' failed
| make: *** [sub-tests-make_first] Error 2

| ERROR: oe_runmake failed

| WARNING:
${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/temp/run.do_compile.82553:1
exit 1 from 'exit 1'
| ERROR: Execution of
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/qtbase/5.14.2+gitAUTOINC+3a6d8df521-r0.arago17/temp/run.do_compile.82553'
failed with exit code 1

ERROR: Task (${home}/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2146 tasks of which 2065 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds
ERROR: Command execution failed: Stopped build

+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Deal:
this problem is casued by the damaged package qtbase, do:
bitbake -c cleanall qtbase.
to clean the package and rerun.

+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

=========================================================================
| PROBLEM SCRIPTION: |
=========================================================================
| collect2: fatal error: ld terminated with signal 9 [Killed]
| compilation terminated.
| cctest.target.mk:206: recipe for target 'Release/cctest' failed
| make[1]: *** [Release/cctest] Error 1
| make[1]: *** Waiting for unfinished jobs....
| rm 497f8524ce51ed4f51f1e0cf89802a9fdc8b7276.intermediate
| Makefile:104: recipe for target 'node' failed
| make: *** [node] Error 2
| ERROR: oe_runmake failed
| WARNING:
${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/nodejs/12.21.0-r0/temp/run.do_compile.3352:1
exit 1 from 'exit 1'
| ERROR:
Execution of
'${home}/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/nodejs/12.21.0-r0/temp/run.do_compile.3352'
failed with exit code 1

ERROR: Task (${home}/sources/meta-openembedded/meta-oe/recipes-devtools/nodejs/nodejs_12.21.0.bb:do_compile) failed with exit code '1'

+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Deal:
this problem is casued by the damaged package nodejs, do:
bitbake -c cleanall nodejs.
to clean the package and rerun.

+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++





Below is the log

U-Boot SPL 2021.01-g15769936a5 (Aug 16 2022 - 06:54:30 +0000)
Trying to boot from MMC1


U-Boot 2021.01-g15769936a5 (Aug 16 2022 - 06:54:30 +0000)

CPU : AM335X-GP rev 1.0
Model: TI AM335x EVM-SK
DRAM: 256 MiB
WDT: Started with servicing (60s timeout)
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... *** Warning - bad CRC, using default environment

<ethaddr> not set. Validating first E-fuse MAC
Net: eth2: ethernet@4a100000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
574 bytes read in 3 ms (186.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
Found /extlinux/extlinux.conf
Retrieving file: /extlinux/extlinux.conf
177 bytes read in 4 ms (43 KiB/s)
1: Arago
Retrieving file: /extlinux/../zImage
4989440 bytes read in 379 ms (12.6 MiB/s)
append: root=PARTUUID=91ffca65-02 rootwait rw console=ttyO0,115200n8,115200
Retrieving file: /extlinux/../am335x-evmsk.dtb
95839 bytes read in 12 ms (7.6 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8df22000, end 8df3c65e ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.10.65-gdcc6bedb2c (oe-user@oe-host) (arm-none-linux-gnueabihf-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 PREEMPT Sun Aug 14 07:14:33 UTC 2022
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x EVM-SK
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] Zone ranges:
[ 0.000000] Normal [mem 0x0000000080000000-0x000000008fefffff]
[ 0.000000] HighMem empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000008fefffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000008fefffff]
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES1.0 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64706
[ 0.000000] Kernel command line: root=PARTUUID=91ffca65-02 rootwait rw console=ttyO0,115200n8,115200
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 192672K/261120K available (10240K kernel code, 693K rwdata, 3380K rodata, 1024K init, 281K bss, 19296K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
[ 0.000000] random: get_random_bytes called from start_kernel+0x30c/0x4c8 with crng_init=0
[ 0.000000] TI gptimer clocksource: always-on /ocp/interconnect@44c00000/segment@200000/target-module@31000
[ 0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000035] clocksource: dmtimer: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000455] TI gptimer clockevent: 24000000 Hz at /ocp/interconnect@48000000/segment@0/target-module@40000
[ 0.001794] Console: colour dummy device 80x30
[ 0.001845] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.001854] This ensures that you still see kernel messages. Please
[ 0.001862] update your kernel commandline.
[ 0.001926] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.120530] pid_max: default: 32768 minimum: 301
[ 0.120728] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.120750] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.121799] CPU: Testing write buffer coherency: ok
[ 0.121890] CPU0: Spectre v2: using BPIALL workaround
[ 0.122940] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.123124] rcu: Hierarchical SRCU implementation.
[ 0.123246] EFI services will not be available.
[ 0.123666] devtmpfs: initialized
[ 0.139529] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.139853] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.139882] futex hash table entries: 256 (order: -1, 3072 bytes, linear)
[ 0.144133] pinctrl core: initialized pinctrl subsystem
[ 0.145290] DMI not present or invalid.
[ 0.145843] NET: Registered protocol family 16
[ 0.148584] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.168527] l3-aon-clkctrl:0000:0: failed to disable
[ 0.170029] thermal_sys: Registered thermal governor 'fair_share'
[ 0.170046] thermal_sys: Registered thermal governor 'bang_bang'
[ 0.170063] thermal_sys: Registered thermal governor 'step_wise'
[ 0.170073] thermal_sys: Registered thermal governor 'user_space'
[ 0.170579] cpuidle: using governor ladder
[ 0.170638] cpuidle: using governor menu
[ 1.897639] No ATAGs?
[ 1.897675] hw-breakpoint: debug architecture 0x4 unsupported.
[ 1.932039] v1_8d: supplied by vbat
[ 1.932956] v3_3d: supplied by vbat
[ 1.934379] iommu: Default domain type: Translated
[ 1.937225] SCSI subsystem initialized
[ 1.937871] mc: Linux media interface: v0.10
[ 1.937929] videodev: Linux video capture interface: v2.00
[ 1.938065] pps_core: LinuxPPS API ver. 1 registered
[ 1.938079] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.938108] PTP clock support registered
[ 1.938193] EDAC MC: Ver: 3.0.0
[ 1.940017] Advanced Linux Sound Architecture Driver Initialized.
[ 1.942073] clocksource: Switched to clocksource dmtimer
[ 1.951787] NET: Registered protocol family 2
[ 1.952030] IP idents hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 1.953305] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear)
[ 1.953353] TCP established hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 1.953389] TCP bind hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 1.953423] TCP: Hash tables configured (established 2048 bind 2048)
[ 1.953568] UDP hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 1.953595] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 1.953800] NET: Registered protocol family 1
[ 1.954462] RPC: Registered named UNIX socket transport module.
[ 1.954482] RPC: Registered udp transport module.
[ 1.954491] RPC: Registered tcp transport module.
[ 1.954500] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.954523] PCI: CLS 0 bytes, default 64
[ 1.955681] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 1.957254] Initialise system trusted keyrings
[ 1.957667] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 1.962938] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.963874] NFS: Registering the id_resolver key type
[ 1.963935] Key type id_resolver registered
[ 1.963947] Key type id_legacy registered
[ 1.964070] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.964086] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 1.964134] ntfs: driver 2.1.32 [Flags: R/O].
[ 1.964889] Key type asymmetric registered
[ 1.964915] Asymmetric key parser 'x509' registered
[ 1.964978] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 1.964994] io scheduler mq-deadline registered
[ 1.965005] io scheduler kyber registered
[ 2.462142] random: fast init done
[ 2.499046] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 2.645113] debugfs: Directory '49000000.dma' with parent 'dmaengine' already present!
[ 2.645169] edma 49000000.dma: TI EDMA DMA engine driver
[ 2.695372] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 2.700431] pwm-backlight backlight: supply power not found, using dummy regulator
[ 2.765320] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 2.771217] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 20, base_baud = 3000000) is a 8250
[ 3.459909] printk: console [ttyS0] enabled
[ 3.468158] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 3.474730] random: crng init done
[ 3.498474] panel-simple panel: supply power not found, using dummy regulator
[ 3.523284] brd: module loaded
[ 3.535235] loop: module loaded
[ 3.544888] libphy: Fixed MDIO Bus: probed
[ 3.612181] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 3.619897] libphy: 4a101000.mdio: probed
[ 3.637264] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Qualcomm Atheros AR8031/AR8033
[ 3.647476] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Qualcomm Atheros AR8031/AR8033
[ 3.658707] cpsw-switch 4a100000.switch: initialized cpsw ale version 1.4
[ 3.665648] cpsw-switch 4a100000.switch: ALE Table size 1024
[ 3.671470] cpsw-switch 4a100000.switch: cpts: overflow check period 500 (jiffies)
[ 3.679177] cpsw-switch 4a100000.switch: CPTS: ref_clk_freq:250000000 calc_mult:2147483648 calc_shift:29 error:0 nsec/sec
[ 3.690307] cpsw-switch 4a100000.switch: Detected MACID = d4:94:a1:89:76:f7
[ 3.697374] cpsw-switch 4a100000.switch: Detected MACID = d4:94:a1:89:76:f8
[ 3.706224] cpsw-switch 4a100000.switch: initialized (regs 0x4a100000, pool size 256) hw_ver:0019010C 1.12 (0)
[ 3.717722] i2c /dev entries driver
[ 3.724999] cpuidle: enable-method property 'ti,am3352' found operations
[ 3.732693] sdhci: Secure Digital Host Controller Interface driver
[ 3.738914] sdhci: Copyright(c) Pierre Ossman
[ 3.744918] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.753801] sdhci-omap 481d8000.mmc: supply vqmmc not found, using dummy regulator
[ 3.763450] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.786562] davinci-mcasp 4803c000.mcasp: IRQ common not found
[ 3.795101] NET: Registered protocol family 10
[ 3.801300] Segment Routing with IPv6
[ 3.805243] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.812036] NET: Registered protocol family 17
[ 3.817065] Key type dns_resolver registered
[ 3.822284] omap_voltage_late_init: Voltage driver support not added
[ 3.829470] Loading compiled-in X.509 certificates
[ 3.851693] OMAP GPIO hardware version 0.1
[ 3.892382] tps65910 0-002d: No interrupt support, no core IRQ
[ 3.900442] vrtc: supplied by vbat
[ 3.907470] vio: supplied by vbat
[ 3.912746] vdd_mpu: supplied by vbat
[ 3.918211] vdd_core: supplied by vbat
[ 3.924705] vdig1: supplied by vbat
[ 3.929560] vdig2: supplied by vbat
[ 3.934440] vpll: supplied by vbat
[ 3.939196] vdac: supplied by vbat
[ 3.943978] vaux1: supplied by vbat
[ 3.948828] vaux2: supplied by vbat
[ 3.953727] vaux33: supplied by vbat
[ 3.958802] vmmc: supplied by vbat
[ 3.963856] vbb: supplied by vbat
[ 3.969158] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 3.985476] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0
[ 4.038348] Console: switching to colour frame buffer device 60x34
[ 4.061148] tilcdc 4830e000.lcdc: [drm] fb0: tilcdcdrmfb frame buffer device
[ 4.071861] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22)
[ 4.086873] input: gpio_buttons0 as /devices/platform/gpio_buttons0/input/input0
[ 4.096284] sdhci-omap 481d8000.mmc: supply vqmmc not found, using dummy regulator
[ 4.104171] sdhci-omap 48060000.mmc: Got CD GPIO
[ 4.109086] sdhci-omap 48060000.mmc: supply vqmmc not found, using dummy regulator
[ 4.123693] ALSA device list:
[ 4.126705] No soundcards found.
[ 4.205425] mmc0: SDHCI controller on 48060000.mmc [48060000.mmc] using External DMA
[ 4.287535] mmc1: SDHCI controller on 481d8000.mmc [481d8000.mmc] using External DMA
[ 4.296065] mmc0: new high speed SDHC card at address e624
[ 4.302617] Waiting for root device PARTUUID=91ffca65-02...
[ 4.309873] mmcblk0: mmc0:e624 SU04G 3.69 GiB
[ 4.315258] sdhci-omap 481d8000.mmc: card claims to support voltages below defined range
[ 4.326198] mmcblk0: p1 p2
[ 4.365627] mmc1: new SDIO card at address 0001
[ 6.045521] EXT4-fs (mmcblk0p2): recovery complete
[ 6.052987] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 6.061299] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 6.069621] devtmpfs: mounted
[ 6.075668] Freeing unused kernel memory: 1024K
[ 6.081245] Run /sbin/init as init process
[ 6.440210] systemd[1]: System time before build time, advancing clock.
[ 6.479735] systemd[1]: systemd 244 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 6.502893] systemd[1]: Detected architecture arm.

Welcome to Arago 2021.09!

[ 6.544103] systemd[1]: Set hostname to <am335x-evm>.
[ 7.710997] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 7.723736] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 7.737937] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 7.775480] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 7.817257] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 7.853315] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 7.893666] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 7.934292] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 7.972658] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 8.012962] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 8.053422] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 8.098075] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 8.133002] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 8.197812] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 8.234119] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 8.332997] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 8.343987] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 8.384181] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 8.425939] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 8.465279] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 8.503537] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 8.544885] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[ 8.564684] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 8.601753] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 8.664137] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 8.684337] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[ 8.710404] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 8.771233] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 8.813593] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 8.854815] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 8.934133] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 8.987575] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 9.011943] cryptodev: loading out-of-tree module taints kernel.
Starting Remount Root and Kernel File Systems...
[ 9.042885] cryptodev: driver 1.10 loaded.
[ 9.060554] systemd[1]: Starting udev Coldplug all Devices...
[ 9.140072] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting udev Coldplug all Devices...
[ 9.231017] systemd[1]: Started Start psplash boot splash screen.
[ OK ] Started Start psplash boot splash screen.
[ 9.293620] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 9.314223] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 9.344097] systemd[1]: Mounted Kernel Debug File System.
[ OK ] Mounted Kernel Debug File System.
[ 9.363775] systemd[1]: Mounted Temporary Directory (/tmp).
[ OK ] Mounted Temporary Directory (/tmp).
[ 9.402807] systemd[1]: Started Load Kernel Modules.
[ OK ] Started Load Kernel Modules.
[ 9.432999] systemd[1]: Started Remount Root and Kernel File Systems.
[ OK ] Started Remount Root and Kernel File Systems.
[ 9.465124] systemd[1]: Condition check resulted in FUSE Control File System being skipped.
[ 9.527261] systemd[1]: Mounting Kernel Configuration File System...
Mounting Kernel Configuration File System...
[ 9.600014] systemd[1]: Started Start psplash-systemd progress communication helper.
[ OK ] Started Start psplash-syst…progress communication helper.
[ 9.676869] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped.
[ 9.738000] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 9.762815] systemd[1]: Condition check resulted in Create System Users being skipped.
[ 9.819707] systemd[1]: Starting Create Static Device Nodes in /dev...
Starting Create Static Device Nodes in /dev...
[ 9.894967] systemd[1]: Mounted Kernel Configuration File System.
[ OK ] Mounted Kernel Configuration File System.
[ 9.954143] systemd[1]: Started Apply Kernel Variables.
[ OK ] Started Apply Kernel Variables.
[ 10.014360] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting Flush Journal to Persistent Storage...
[ 10.378814] systemd-journald[91]: Received client request to flush runtime journal.
Starting udev Kernel Device Manager...
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
[ OK ] Started Flush Journal to Persistent Storage.
Starting Load/Save Random Seed...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started udev Kernel Device Manager.
[ 13.245825] remoteproc remoteproc0: wkup_m3 is available
[ OK ] Created slice system-systemd\x2dbacklight.slice.
Starting Load/Save Screen …ness of backlight:backlight...
[ OK ] Started Load/Save Screen B…htness of backlight:backlight.
[ 13.996392] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 14.010661] omap_rtc 44e3e000.rtc: already running
[ 14.123838] omap_rtc 44e3e000.rtc: registered as rtc0
[ 14.128979] omap_rtc 44e3e000.rtc: setting system clock to 2022-08-11T09:50:33 UTC (1660211433)
[ OK ] Started udev Coldplug all Devices.
Starting udev Wait for Complete Device Initialization...
[ 15.022785] remoteproc remoteproc0: powering up wkup_m3
[ 15.071502] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 243280
[ 15.142578] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 15.142607] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 15.653790] am335x-phy-driver 47401300.usb-phy: supply vcc not found, using dummy regulator
[ 15.746999] usbcore: registered new interface driver usbfs
[ 15.755138] am335x-phy-driver 47401b00.usb-phy: supply vcc not found, using dummy regulator
[ 15.797967] usbcore: registered new interface driver hub
[ 15.834592] usbcore: registered new device driver usb
[ 15.961273] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 16.113713] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 16.252634] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 16.260970] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 16.432537] usb usb1: Product: MUSB HDRC host driver
[ 16.437556] usb usb1: Manufacturer: Linux 5.10.65-gdcc6bedb2c musb-hcd
[ 16.562379] usb usb1: SerialNumber: musb-hdrc.0
[ 16.625254] hub 1-0:1.0: USB hub found
[ 16.652467] hub 1-0:1.0: 1 port detected
[ 16.748357] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 16.857908] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 16.962604] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 16.970961] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 17.157007] usb usb2: Product: MUSB HDRC host driver
[ 17.162028] usb usb2: Manufacturer: Linux 5.10.65-gdcc6bedb2c musb-hcd
[ 17.274289] usb usb2: SerialNumber: musb-hdrc.1
[ 17.306342] hub 2-0:1.0: USB hub found
[ 17.392285] hub 2-0:1.0: 1 port detected
[ 19.468961] PM: bootloader does not support rtc-only!
[ 19.567871] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 19.704554] omap-sham 53100000.sham: will run requests pump with realtime priority
[ 19.725108] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 19.790911] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 19.820131] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
[ *** ] (2 of 2) A start job is running for…ice Initialization (19s / 3min 6s)
[ 27.667882] TI-am335x-tsc TI-am335x-tsc.0.auto: ti,charge-delay not specified
[ 27.766459] input: ti-tsc as /devices/platform/ocp/44c00000.interconnect/44c00000.interconnect:segment@200000/44e0d000.target-mod[ OK ] Found device /dev/disk/by-uuid/37E4-397A.
[ 28.483114] 4a328000.serial: ttyS1 at MMIO 0x4a328000 (irq = 72, base_baud = 12000000) is a 16550A
[ 28.586216] remoteproc remoteproc1: 4a334000.pru is available
[ 28.656177] remoteproc remoteproc2: 4a338000.pru is available
[ OK ] Started udev Wait for Complete Device Initialization.
[ OK ] Created slice system-weston.slice.
[ OK ] Reached target Hardware activated USB gadget.
[ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
Mounting /boot...
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 31.745693] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Mounted /boot.
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Save/Restore Sound Card State...
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
Starting Reboot and dump vmcore via kexec...
Starting rc.pvr.service...
Starting Login Service...
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ 34.191650] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[ OK ] Started Reboot and dump vmcore via kexec.
[ 34.402318] lis3_reg: disabling
[ 34.405519] v1_8d: disabling
[ 34.408414] v3_3d: disabling
[ 34.442328] vwl1271: disabling
[ OK ] Started rc.pvr.service.
[ OK ] Reached target Network (Pre).
[ OK ] Reached target Sound Card.
Starting Network Service...
Starting weston.service...
[ OK ] Started weston.service.
Starting Matrix GUI...
Starting telnetd.service...
[ OK ] Started Matrix GUI.
[ OK ] Started telnetd.service.
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
[ 35.888469] cpsw-switch 4a100000.switch: starting ndev. mode: dual_mac
Starting Network Name Resolution...
[ 36.106994] Qualcomm Atheros AR8031/AR8033 4a101000.mdio:01: attached PHY driver [Qualcomm Atheros AR8031/AR8033] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL)
[ 36.376707] cpsw-switch 4a100000.switch: starting ndev. mode: dual_mac
[ 36.548997] Qualcomm Atheros AR8031/AR8033 4a101000.mdio:00: attached PHY driver [Qualcomm Atheros AR8031/AR8033] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
[ OK ] Started Login Service.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Started Permit User Sessions.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston Wayland Compositor...
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
[ 44.195379] cryptd: max_cpu_qlen set to 1000

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org am335x-evm ttyS0

Arago 2021.09 am335x-evm ttyS0

am335x-evm login: ***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gstreamer1.0-libav
gzip
less
libasm1
libbfd
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libreadline-dev
libreadline8
libunistring2
m4-dev
m4
make
nettle
parted
pdm-anomaly-detection
tar
which

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************

Thanks.
Rgds
Shine