Part Number: SK-AM64
Hello,
I would like to check Timesync (PTP) example from SDK (mcu_plus_sdk_am64x_08_02_00_31) but it seems that it doesn't work correctly for me - it doesn't return PTP packets that were sent to it..
I started the example in Code Composer Studio and loaded it to R5 core:
Then I sent PTPv2 packet from ptp4l application. It have tried the same configuration of PTP as here. In Wireshark I can see the ptp packets on the interface that is connected directly to AM64 SK board:
but there is no response from the AM64 SK board.
I can add that the ethernet cable is connected to Port 1 of the board and application recognizes it saying: "MAC Port 1: link up" so it seems that physically connection is ok.
Any idea what is wrong?