Hello Champs,
Currently, when debugging J7200 DEMOProject (BOOT_APP_MCU_RTOS), all CAN (8 channels) are configured in the same way, but:
1. The main domain CAN12 is blocked, please see the below for the waveform of TX;
2. After primary domain CAN15 is initialized and written to the base address 0x02698000, no packets are sent from all CAN, and the controller current is coded from 7500mA to 6800mA.
Thanks.
Rgds
Shine