This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: About DSS (Display Subsystem) of AM62x

Part Number: AM625
Other Parts Discussed in Thread: AM623

Hi experts,

There is a difference between AM625x and AM623x with/without GPU, but I understand that both of them support Linux and can display screens.

Is it correct that as for the difference between with and without GPU, does it mean that 3D polygon display is not possible?
Or is it simply that the processing is slower because the 3D polygons are done on the CPU side due to the without GPU?

For the AM62xx evaluation board, is there an LCD that can be connected to the LCD connector?
(For example, the LCD kit for AM57xx can be used.)

Best regards,
O.H