This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: TDA4VM-Q1: HS OTP keywrite & booting on HS-FS devices

Part Number: TDA4VM-Q1

Hi experts : 

                   I using RTOS SDK 7.3 and evm HS board.

                   Knowing that OTP keywrite version 8.0 can be well supported, so the OTP keywrite image compiled with sdk8.0 version is used。Other images, all use SDK 7.3

                   With ti local support, I got the two files required by OTP ti_fek_public.pem ti-fs-keywriter.bin

                   I have completed the burning, and the Debug response: 0x0, but according to this, it is not completely sure whether the burning is ok, please check the following log for help to confirm

                   The ti dummy key used for this burn。

                   MCU log:

                   

OTP Keywriter Version: 02.00.00.00 (Sep  7 2022 - 20:44:30)

 OTP Keywriter ver: 21.5.2--v2021.05b (Terrific Lla
OTP_VppEn
**************
Debug:func:test_pmic_appInit,line=1139, pmicConfigData->commMode = 0
***************
test_pmic_i2c_lld_intf_setup(): 493: PMIC_MAIN_INST I2C Setup...
test_pmic_i2c_lld_intf_setup(): 533: done...
**************
Debug:func:Pmic_init,line=581, regVal = 82
***************
I2C1: Passed for address 0x4c !!!
I2C1: Passed for address 0x13 !!!
**************
Debug:func:test_pmic_appInit,line=1189, pmicStatus = 0
***************
INT STAT[0]: 0x00000000
INT STAT[1]: 0x00002002
INT STAT[2]: 0x00000000
INT STAT[3]: 0x00000000

**************
Debug:func:OTP_VppEn,line=98, test_pmic_appInit status = 0
***************
Key programming sequence initialted
Taking OTP certificate from 0x41c73004
Debug response: 0x0

                  M3 log:

                  

debug_response:  0x10000
                                                       0x400002
                                                               0x800004
                                                                       0x4003005
                                                                                0x4401552
                                                                                         0x40000B
                                                                                                 0x800004
                                                                                                         0x4003005
                                                                                                                  0x4401552
                                                                                                                           0x40000D
                                                                                                                                   0x800004
                                                                                                                                           0x20800000
                                                                                                                                                     0x20800001
    0x400002
            0x800004
                    0x4003005
                             0x4401552
                                      0x409031
                                              0x800004
                                                      #
                                                       # Decrypting extensions..
                                                                                #
                                                                                 MPK Options:  0x0
                                                                                                  MEK Options:  0x0
                                                                                                                   MPK Opt P1:  0x0
                                                                                                                                   MPK Opt P2:  0x0
                                                                                                                                                   MEK Opt   :  0x0
        * SMPKH Part 1 BCH code: e050cadb

                                         * SMPKH Part 2 BCH code: c099dd36

                                                                          * SMPK Hash (part-1,2):

                                                                                                 1f6002b07cd9b0b7c47d9ca8d1aae57b8e8784a12f636b2b760d7d98a18f189700

        60dfd0f23e2b0cb10ec7edc7c6edac3d9bdfefe0eddc3fff7fe9ad875195527d00

                                                                          * SMEK BCH code: a0c6de4e

                                                                                                   * SMEK Hash: 92785809a3dfefea57f6bbed642d730ba5d05e601222a72e815bf01ceb3a50f96ab85d282425f684436fabd4c7da624b791da411615035314103cc64e611f532

                                                                                     EXT OTP extension disabled
                                                                                                               MSV extension disabled

                                                                                                                                     * KEY CNT: 01010000

                                                                                                                                                        * KEY REV: 01010000

                SWREV extension disabled

                                        FW CFG REV extension disabled

                                                                     * KEYWR VERSION:  0x20000

                                                                                              #
                                                                                               # Programming Keys..
                                                                                                                   #

                                                                                                                    * MSV:
                                                                                                                           [u32] bch + msv:  0x0
                                                                                                                                                MSV extension disabled
           [u32] bch + msv:  0x0

                                * SWREV:
                                         [u32] SWREV-SYSFW:  0x1
                                                                [u32] SWREV-SBL  :  0x1
                                                                                       SWREV extension disabled
                                                                                                               [u32] SWREV-SYSFW:  0x1
                                                                                                                                      [u32] SWREV-SBL  :  0x1

  * FW CFG REV:
                [u32] SWREV-FW-CFG-REV:  0x1
                                            SWREV SEC BCFG extension disabled
                                                                             [u32] SWREV-FW-CFG-REV:  0x1

                                                                                                         * EXT OTP:
                                                                                                                    EXT OTP extension disabled

                                                                                                                                              * BMPKH, BMEK:
  BMPKH extension disabled
                          BMEK extension disabled

                                                 * SMPKH, SMEK:
                                                                Programmed 11/11 rows successfully
                                                                                                  Programmed 2/2 rows successfully
                                                                                                                                  Programmed 11/11 rows successfully
         Programmed 2/2 rows successfully
                                         Programmed 11/11 rows successfully
                                                                           Programmed 2/2 rows successfully

                                                                                                           * KEYCNT:
                                                                                                                     [u32] keycnt:  0x0
                                                                                                                                       Programmed 2/2 rows successfully
            [u32] keycnt:  0x1

                              * KEYREV:
                                        [u32] keyrev:  0x0
                                                          Programmed 2/2 rows successfully
                                                                                          [u32] keyrev:  0x1

                  I'm not entirely sure the burn is ok because I'm running into a problem。

                 compiler sbl through make -s -j4 BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_mmcsd_img_hlos_hs and copy to SD 

                 Power on and start, sbl can start normally, but cannot load tifs.bin correctly

                 

                 I tried the tifs*.bin under packages/ti/drv/sciclient/soc/V1, but it doesn't solve the problem

                 

                 Generating the corresponding tifs*.bin through the script firmwareHeaderGen.sh also does not work

                

                I can't understand very well, what kind of tifs.bin is needed(dual signed or single signed)


                please give a reasonable solution,thanks a lot!