This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: How gpiochip pin numbers are mapped to schematic?

Part Number: AM6442


Hello

I want to light up the LED connected to the RPI_GPIO0_42 Expansion connector pin using /dev/gpiochip3. How pin numbers listed with the command: gpioinfo 3  map to the pins of the AM6442 processor? On the schematic (https://www.ti.com/lit/pdf/sprr432) the pin RPI_GPIO0_42  is pin R20.

root@am64xx-evm:/sys/class/gpio/gpiochip327# gpioinfo 3
gpiochip3 - 88 lines:
        line   0:      unnamed       unused   input  active-high
        line   1:      unnamed       unused   input  active-high
        line   2:      unnamed       unused   input  active-high
        line   3:      unnamed       unused   input  active-high
        line   4:      unnamed       unused   input  active-high
        line   5:      unnamed       unused   input  active-high
        line   6:      unnamed       unused   input  active-high
        line   7:      unnamed       unused   input  active-high
        line   8:      unnamed       unused   input  active-high
        line   9:      unnamed       unused   input  active-high
        line  10:      unnamed       unused   input  active-high
        line  11:      unnamed       unused   input  active-high
        line  12:      unnamed       unused   input  active-high
        line  13:      unnamed       unused   input  active-high
        line  14:      unnamed       unused   input  active-high
        line  15:      unnamed       unused   input  active-high
        line  16:      unnamed       unused   input  active-high
        line  17:      unnamed       unused   input  active-high
        line  18:      unnamed       unused   input  active-high
        line  19:      unnamed       unused   input  active-high
        line  20:      unnamed       unused   input  active-high
        line  21:      unnamed       unused   input  active-high
        line  22:      unnamed       unused   input  active-high
        line  23:      unnamed       unused   input  active-high
        line  24:      unnamed       unused   input  active-high
        line  25:      unnamed       unused   input  active-high
        line  26:      unnamed       unused   input  active-high
        line  27:      unnamed       unused   input  active-high
        line  28:      unnamed       unused   input  active-high
        line  29:      unnamed       unused   input  active-high
        line  30:      unnamed       unused   input  active-high
        line  31:      unnamed       unused   input  active-high
        line  32:      unnamed       unused   input  active-high
        line  33:      unnamed       unused   input  active-high
        line  34:      unnamed       unused   input  active-high
        line  35:      unnamed       unused   input  active-high
        line  36:      unnamed       unused   input  active-high
        line  37:      unnamed       unused   input  active-high
        line  38:      unnamed       unused   input  active-high
        line  39:      unnamed       unused   input  active-high
        line  40:      unnamed       unused   input  active-high
        line  41:      unnamed       unused   input  active-high
        line  42:      unnamed       unused   input  active-high
        line  43:      unnamed       unused   input  active-high
        line  44:      unnamed       unused   input  active-high
        line  45:      unnamed       unused   input  active-high
        line  46:      unnamed       unused   input  active-high
        line  47:      unnamed       unused   input  active-high
        line  48:      unnamed       unused   input  active-high
        line  49:      unnamed       unused   input  active-high
        line  50:      unnamed       unused   input  active-high
        line  51:      unnamed       unused   input  active-high
        line  52:      unnamed       unused   input  active-high
        line  53:      unnamed       unused   input  active-high
        line  54:      unnamed       unused   input  active-high
        line  55:      unnamed       unused   input  active-high
        line  56:      unnamed       unused   input  active-high
        line  57:      unnamed       unused   input  active-high
        line  58:      unnamed       unused   input  active-high
        line  59:      unnamed       unused   input  active-high
        line  60:      unnamed       unused   input  active-high
        line  61:      unnamed       unused   input  active-high
        line  62:      unnamed       unused   input  active-high
        line  63:      unnamed       unused   input  active-high
        line  64:      unnamed       unused   input  active-high
        line  65:      unnamed       unused   input  active-high
        line  66:      unnamed       unused   input  active-high
        line  67:      unnamed       unused   input  active-high
        line  68:      unnamed       unused   input  active-high
        line  69:      unnamed       unused   input  active-high
        line  70:      unnamed       unused   input  active-high
        line  71:      unnamed       unused   input  active-high
        line  72:      unnamed       unused   input  active-high
        line  73:      unnamed       unused   input  active-high
        line  74:      unnamed       unused   input  active-high
        line  75:      unnamed       unused   input  active-high
        line  76:      unnamed       unused   input  active-high
        line  77:      unnamed       unused   input  active-high
        line  78:      unnamed       unused   input  active-high
        line  79:      unnamed       unused   input  active-high
        line  80:      unnamed       unused   input  active-high
        line  81:      unnamed       unused   input  active-high
        line  82:      unnamed       unused   input  active-high
        line  83:      unnamed       unused   input  active-high
        line  84:      unnamed       unused   input  active-high
        line  85:      unnamed       unused   input  active-high
        line  86:      unnamed       unused   input  active-high
        line  87:      unnamed       unused   input  active-high

Thank you,

Jakub