Hi,
I have a problem with building u-boot and kernel in ubuntu 22.04.
when i running arm-oe-linux-gnueabi-gcc, i get error "error while loading shared libraries: libm.so.6: cannot open shared object file: No such file or directory"
If i directy put library path with environment "export LD_LIBRARY_PATH="/home/......./ti-processor-sdk-linux-omapl138-lcdk-06.03.00.106/linux-devkit/sysroots/x86_64-arago-linux/lib" i get "version `GLIBC_2.34' not found (required by make)"
build-essential libncurses5-dev and other 32-bit libraries already installed.
Any suggestions?