Hello Ti,
I want to build the RT-Linux sd card image for SK-AM62.
Is there any information for the image building?
BR
James
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ti,
I want to build the RT-Linux sd card image for SK-AM62.
Is there any information for the image building?
BR
James
Hi James,
What do you mean by 'build', compile every component from source?
FYI, there is the RT Linux SD card image provided in the Processor SDK RT-Linux v8.4:
https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-BDCgfEXHLk/08.04.01.03/tisdk-default-image-am62xx-evm.wic.xz
It is also packaged in the SDK v8.4 installer:
https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-BDCgfEXHLk/08.04.01.03/ti-processor-sdk-linux-rt-am62xx-evm-08.04.01.03-Linux-x86-Install.bin
Hi James,
if you want to build the SD card image completely from source you need to perform a Yocto build. The "how" is documented in the associated AM62 Processor SDK Linux documentation (current version as of writing this is v8.04), see here https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/08_04_01_03/exports/docs/linux/Overview_Building_the_SDK.html
The key difference for "RT Linux" vs the building images/SDK for the regular Linux is an additional ENV variable named ARAGO_RT_ENABLE=1 that needs to be passed to bitbake. Search for "RT Support" in the page referenced above.
Let me know if this doesn't answer your questions or you have any issues building SD card images etc. from source.
Regards, Andreas