Dear Support:
I have been able to bootup my SK-TDA4VM and run from the SD card and use the console output via minicom - no issues. I have run the setup script./setup from the Linux SDK by following the directions here:
Where I designed that I wanted to bootup via TFTP and use NFS. I have followed all the documentation on what all needs to be done to get NFS running with my Ubuntu v18.04 laptop and can TFTP the necessary files such as:
tftp 0x82000000 Image-j7-evm.bin
tftp 0x81200000 k3-j721e-common-proc-board.dtb
and using the following:
I am able to create my SD card which defaults to using the SD card to bootup the board even though I ran the setup script to tell it to boot from TFTP and use NFS.
Since my board is booting up from the SD card and I want to use NFS, I don't see any example NFS "setenv" statements that I can use to get it running on my board. I have been on the e2e forum and looked at all the NFS posts that are available, but they don't provided details on what are the "setenv" statements I need to execute from boot so that my board will bootup via NFS. Can you provide this for me so I can enter the necessary variables and "saveenv" so my board will bootup using NFS?
And so I don't trash any existing environment variables, please provide the necessary "setenv" values I need to use so that if I want to go back to booting up from my SD card, I can enter those values and boot my board via the SD card.
Thanks,
Tim