Hi everyone,
I am trying to build adc_test project for idk AM437x evaluation board from C:\ti\pdk_am437x_1_0_17\packages\ti\starterware\examples\adc
I was trying to gmake the project; however, it only generates binary files including .out and .bin files but not .ccsproject (which allows me to import to CCS project)
Therefore, I decided to open UART_BasicExample_idkAM437x_armExampleProject and copy adc_test.c file into the Uart project.
After adding additional paths including:
I also added: cpu.c, gic.c, and tsc_adc_ss.c file into my project.
I finally got my project built and run the adc_test.c project on my IDK Am437x eval board.
However, the code is stopped at this while loop:
I went back and checked to make sure ADC0 is enable in the Pinmux as:
I suspect that the interrupt never happens and causes the code stuck in the while loop above.
I wonder if I am missing any configurations for the ADC which is caused this issue.
That would be great if I can have any suggestions or hint on this. Or maybe a better way to import the project.
Thank you for reading my post.
Sincerely,
Minh Vo