Hi TI!
I need to use pins A19 and B19 as UART5_TX and UART5_RX respectively as the linux command output.
These pins are also used to configure the boot source. So they have two external resistors (pull down) connected to configure the boot source.
Can this generate a conflict?
I imagine that the UART5_RX (B19) must be connected (physically) to an external device after boot, otherwise there will be 3.3V on the B19 pin at power on and it will not boot.
Is this analysis correct?
Thanks very much.
Best Regards.