Other Parts Discussed in Thread: DRA821
Hi,
We are developing a new product called Automotion Server that is one is a evolution on a existing product.
The new product will be based on DRA821 processor.
The existing product is using a co-processor which main tasks are to handle the reset and supervisory of the main processor.
So when the product is powered up the co-processor is checking that all the main power input to the product is OK and then resets the main processor.
It also continuously monitors the main processor during runtime where the main processor needs to kick a watchdog in the co-processor and if this fail the co-processor will initiate a power failure/backup step.
My question for the new product where we will use the DRA821 processor if the R5F cores inside the DRA821 can be used instead of a seperate co-processor.
Are the R5F cores completly isolated from the other cores(Dual A72) and domains and can be powered and reset seperatly ?
I would like to use the R5F cores to monitor the power input with an ADC and if the power input is OK the R5F cores will pull the rest of the processor domains out of reset.
The R5F cores will need to continously monitor the other domains during runtime and if the the domains hangs the R5F core will initialize a controlled power down.
It his possible to use the R5F cores like this.
Thanks!
Regards
Goran