Hi,
Couple of questions below on the DRA829V processor.
Q1; Is it possible to run 2 superspeed USB ports simultaneously on one serdes block?
We would like to support two USB Host ports from one Serdes block instead of using one USB 3.0 and need to add and external USB Hub like TUS8020.
We know the DRA829V processor has another USB 3.0 Controller but that one is already used for another USB Type-C connector.
Q2; Does the MLB block still need power even if it is not used? should the power rails VDDA_1P8_MLB and VDDA_0P8_PLL_MLB be powered.
-Q3;Same question for the power rails used for this functions CSI, MMC1, MMC2, UFS, RGMII5 and -6 (VDDSHV3 and 4), MCU_RGMII (VDDSHV_MCU), SD card (VDDSHV5).
Should blocks that are not used still be powered? Are there any blocks that can be not powered if not used?
Thanks!
Regards
Goran