This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Montavista 2.6.18_pro500 on DM6446 and ALSA Problem



Hi,

I have a DM6446 EVM with ALSA support, DaVinci Sound Driver and TLV320AIC33 support built-in in my kernel 2.6.18_pro500. Despite this, when booting, no soundcard is detected, as here reported:

aic33 mclk=27MHz
davinci mcbsp&aic33 initializing...
aic33:set left mic volume to: 50 set right mic volume to: 50
set left volume to: 50   set right volume to: 50
aic33: Enabling line in
set left igain to:50    Set right igain to: 50
set left ogain to: 100    Set right ogain to: 100
aic33:set left mic volume to: 50 set right mic volume to: 50
set left volume to: 50   set right volume to: 50
aic33: Enabling line in
set left igain to:50    Set right igain to: 50
set left ogain to: 100    Set right ogain to: 100
mmcblk0: mmc0:0260 NCard 984064KiB
 mmcblk0: p1 p2
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
ALSA device list:
  No soundcards found.

In fact, I got the same output if using alsaconf or amixer.

Any idea how to get rid of this?

 

Thanks!

Gab