This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMOMAPL138B-HIREL: UPP with Independent TX and RX data lines

Part Number: SMOMAPL138B-HIREL
Other Parts Discussed in Thread: OMAPL138

HI Team,

we have designed custom board with OMAPL138 and FPGA where both are connected via UPP interface.
Both DSP and FPGA needs to send and receive 16bit or 8 Bit data and planning to use in DUPLEX 1 mode, where CH-A transmits and CH-B receives in DSP.

We have the following queries regarding the UPP communication,

1. Is it possible to communicate with FPGA and DSP simulatenously. I assume UPP control siganls are independent (WAIT, START, ENABLE and CLOCK), hence we will not face issue on these signals.
But for data can we split the 16 bit data lines to dedicate 8 bit each for FPGA and DSP Transmission??