Other Parts Discussed in Thread: TDA4VM
Dear TI ,
I want to use six 30fps 8M cameras in TDA4VM systems. Those cameras have isp functions inside and output yuv422 data format. So the total data rate is 8M*30fps*8bits=1920Mbps(1.92Gbps). One TDA4VM have two CSI2.0 4L RX interface.Each CSI2.0 4L can support 2.5Gbps*4= 10Gbps. So based on the compute above, the TDA4VM have the the ability to support six 30fps 8M yuv422 data format camera moudles. I want to know is my description above right?
Thanks very much!