Hi,
with the newest version of MCU-Plus SDK 08.05.00.24 the example "Enet Layer 2 CPSW " doesn't work anymore on SK-AM64x. Example works in SDK-Version 08.04.00.17.
Here's the output from Debug-UART:
========================== Layer 2 CPSW Test ========================== Init all peripheral clocks ---------------------------------------------- Enabling clocks! Create RX tasks ---------------------------------------------- cpsw-3g: Create RX task Open all peripherals ---------------------------------------------- cpsw-3g: Open enet EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:1 From 4 To 3 Init all configs ---------------------------------------------- cpsw-3g: init config Mdio_open: MDIO Manual_Mode enabled EnetRm_open: Resource partition validation failed: -3 EnetMod_open: cpsw3g.rm: Failed to open: -3 Cpsw_openInternal: Failed to open RM: -3 Assertion @ Line: 984 in /home/gtbldadm/nightlybuilds/mcupsdk_internal/jenkins/mcu_plus_sdk_am64x_08_05_00_24/source/networking/enet/core/src/per/V1/cpsw.c: hCpsw->hRxRsvdFlow != NULL
BTW: I am talking about MCU-PLUS-SDK-AM64X, but I cannot select this part number when creating a thread ...