Other Parts Discussed in Thread: TEST2
Hello Champs,
HW: customer own board with dp83822
SW: linux processor SDK 07-03-00-005
Customer configured sysboot bit7-bit0 to 011 01000 to ethernet boot. He setup the network boot according to below link.
https://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/How_to_Guides/Host/How_to_Setup_Ubuntu_1404_Network_Boot.html
But it prompted below error message:
U-Boot SPL 2020.01-g9d3aef5fd0-dirty (Jan 12 2023 - 14:42:14 +0800)
Trying to boot from eth device
Could not get PHY for eth_cpsw: addr 0
Warning: eth_cpsw using MAC address from ROM
eth0: eth_cpsw
boot net loop test
boot net loop test2
boot net test1
Problem booting with BOOTP
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Below is the host log
threshold, reply with unaltered, existing lease for 192.168.2.3
Jan 12 09:44:47 linux dhcpd[1539]: BOOTREQUEST from 6c:30:2a:c0:83:f1 via enp0s3
Jan 12 09:44:47 linux dhcpd[1539]: BOOTREPLY on 192.168.2.3 to 6c:30:2a:c0:83:f1 via enp0s3
Jan 12 09:44:47 linux atftpd[1547]: Serving u-boot-spl-restore.bin to 192.168.2.3:1234
Thanks
Regards,
Shine