This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: Where's tidl_tools on the board

Part Number: SK-TDA4VM

Hi team,

Here's an issue from the customer may need your help:

When using the official onnxrt_ep.py inference model on the PC side, there is a path where tidl_tools_path is set to the tidl_tools folder. Use tidl_tools_path of the onnxrt_ep.py inference model on development board, which was previously set to "".

1) Is tidl_tools used on the development board? If so, where is this folder?

2) onnxrt_ep.py, common_utils.py, onnx_main.cpp, and onnxrt_ep.py, common_utils.py, are officially available on the PC side, as well as on the board. Does the contents of onnx_main.cpp and the code run the same?

Could you help check this case? Thanks.

Best Regards,

Cherry