Hi team,
Here's an issue from the customer may need your help:
When using the official onnxrt_ep.py inference model on the PC side, there is a path where tidl_tools_path is set to the tidl_tools folder. Use tidl_tools_path of the onnxrt_ep.py inference model on development board, which was previously set to "".
1) Is tidl_tools used on the development board? If so, where is this folder?
2) onnxrt_ep.py, common_utils.py, onnx_main.cpp, and onnxrt_ep.py, common_utils.py, are officially available on the PC side, as well as on the board. Does the contents of onnx_main.cpp and the code run the same?
Could you help check this case? Thanks.
Best Regards,
Cherry