Team,
From the datasheet it's not clear if the two R5F cores are from the same cluster, or from separate ones. So can the two R5F cores in AM2632 operate in lockstep mode?
Thanks,
Robert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
From the datasheet it's not clear if the two R5F cores are from the same cluster, or from separate ones. So can the two R5F cores in AM2632 operate in lockstep mode?
Thanks,
Robert
Hi,
Please expect the delay in response due to weekend.
Thanks
Hi Robert
There are two R5 clusters:
R50 and R51.
R50 cluster has two cores:
R50_0 and R50_1
Lockstep mode:
When this cluster is configured for lockstep mode, only one core can be used - R50_0.
R50_1 is disabled and cannot be connected.
Same is applicable for he R51 cluster in lockstep mode.
More information is available here:
e2e.ti.com/.../faq-am2634-how-to-choose-setup-the-dual-core-with-lockstep-feature
Thanks & regards
Sri Vidya
Hi Sri Vidya,
The question is about AM2632! This device only has two cores.
So are the two cores from one cluster and can operate in lockstep mode?
Or are the two AM2632 A53 cores from different clusters and therefore can't be use in lockstep?
Thanks,
Robert
Hi Robert
The two cores in AM2632 belong to two different clusters.
Hence the two cores are always and only in lockstep mode. It is a Dual Lockstep core.
Thanks & Regards
Sri Vidya