$ MACHINE=am62xx-evm bitbake tisdk-default-image -c populate_sdk
Loading cache: 100% |###############################################################################################################################################################| Time: 0:00:01
Loaded 8446 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: Resolving any missing task queue dependencies
NOTE: Resolving any missing task queue dependencies
NOTE: Resolving any missing task queue dependencies
NOTE: Resolving any missing task queue dependencies
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.46.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "aarch64-linux"
MACHINE = "am62xx-evm"
DISTRO = "jome"
DISTRO_VERSION = "2021.09"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta-processor-sdk = "HEAD:4d3a4e5f476b257405946c5aa222c02fc7565cfb"
meta-arago-distro
meta-arago-extras = "HEAD:dc749e9898eb1594c1289406e908ca62b3b7b077"
meta-qt5 = "HEAD:5ef3a0ffd3324937252790266e2b2e64d33ef34f"
meta-virtualization = "HEAD:beea119eb529b4a11f266004aee8b548427aea39"
meta-networking
meta-python
meta-oe
meta-gnome
meta-filesystems
meta-multimedia = "HEAD:7203130ed8b58c0df75cb72222ac2bcf546bce44"
meta-ti = "HEAD:6763a269b0398aa70ddfa9bece73e17a92849a9e"
meta-xxxxx = "HEAD:f59200309ea97748b0295c3e25eb48252a4c7480"
meta-arm
meta-arm-toolchain = "HEAD:c4f04f3fb66f8f4365b08b553af8206372e90a63"
meta = "HEAD:408bf1b4bb4f4ed126c17fb3676f9fa0513065ba"
Build Configuration:
BB_VERSION = "1.46.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am62xx-evm-k3r5"
DISTRO = "jome"
DISTRO_VERSION = "2021.09"
TUNE_FEATURES = "arm armv7a vfp thumb callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:4d3a4e5f476b257405946c5aa222c02fc7565cfb"
meta-arago-distro
meta-arago-extras = "HEAD:dc749e9898eb1594c1289406e908ca62b3b7b077"
meta-qt5 = "HEAD:5ef3a0ffd3324937252790266e2b2e64d33ef34f"
meta-virtualization = "HEAD:beea119eb529b4a11f266004aee8b548427aea39"
meta-networking
meta-python
meta-oe
meta-gnome
meta-filesystems
meta-multimedia = "HEAD:7203130ed8b58c0df75cb72222ac2bcf546bce44"
meta-ti = "HEAD:6763a269b0398aa70ddfa9bece73e17a92849a9e"
meta-xxxxx = "HEAD:f59200309ea97748b0295c3e25eb48252a4c7480"
meta-arm
meta-arm-toolchain = "HEAD:c4f04f3fb66f8f4365b08b553af8206372e90a63"
meta = "HEAD:408bf1b4bb4f4ed126c17fb3676f9fa0513065ba"
Initialising tasks: 100% |##########################################################################################################################################################| Time: 0:00:08
Sstate summary: Wanted 5 Found 5 Missed 0 Current 1774 (100% match, 100% complete)
NOTE: Executing Tasks
ERROR: tisdk-default-image-1.0-r0.tisdk1 do_populate_sdk: Unable to install packages. Command '/xxxx/AM62x/sdk/test/build/build/arago-tmp-external-arm-glibc/work/am62xx_evm-linux/tisdk-default-image/1.0-r0.tisdk1/recipe-sysroot-native/usr/bin/opkg --volatile-cache -f /xxxx/AM62x/sdk/test/build/build/arago-tmp-external-arm-glibc/work/am62xx_evm-linux/tisdk-default-image/1.0-r0.tisdk1/opkg.conf -t /xxxx/AM62x/sdk/test/build/build/arago-tmp-external-arm-glibc/work/am62xx_evm-linux/tisdk-default-image/1.0-r0.tisdk1/temp/ipktemp/ -o /xxxx/AM62x/sdk/test/build/build/arago-tmp-external-arm-glibc/work/am62xx_evm-linux/tisdk-default-image/1.0-r0.tisdk1/sdk/image/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/aarch64-linux --force_postinstall --add-ignore-recommends ti-llvm3.6-dev --add-ignore-recommends opencl-monitor-dev --add-ignore-recommends libulm-dev --add-ignore-recommends gdbserver-c6x-dev --add-ignore-recommends coreutils --add-ignore-recommends coreutils-dev --add-ignore-recommends busybox-syslog install build-essential docker git libcamera linux-libc-headers-dev opkg packagegroup-arago-base packagegroup-arago-base-tisdk packagegroup-arago-console packagegroup-arago-tisdk-addons packagegroup-arago-tisdk-addons-extra packagegroup-arago-tisdk-amsdk packagegroup-arago-tisdk-connectivity packagegroup-arago-tisdk-crypto packagegroup-arago-tisdk-graphics packagegroup-arago-tisdk-gtk packagegroup-arago-tisdk-hmi packagegroup-arago-tisdk-matrix packagegroup-arago-tisdk-matrix-extra packagegroup-arago-tisdk-multimedia packagegroup-arago-tisdk-qte packagegroup-core-boot packagegroup-core-standalone-sdk-target packagegroup-core-tools-debug packagegroup-dl psplash resize-rootfs run-postinsts systemd-initramfs target-sdk-provides-dummy ti-analytics ti-demos ti-test' returned 1:
Collected errors:
* Solver encountered 1 problem(s):
* Problem 1/1:
* - nothing provides libatomic-dev needed by packagegroup-core-standalone-sdk-target-1.0-r8.aarch64
*
* Solution 1:
* - do not ask to install a package providing packagegroup-core-standalone-sdk-target
Disfavor package: busybox-syslog
Disfavor package: coreutils-dev
Disfavor package: coreutils
ERROR: Logfile of failure stored in: /xxxx/AM62x/sdk/test/build/build/arago-tmp-external-arm-glibc/work/am62xx_evm-linux/tisdk-default-image/1.0-r0.tisdk1/temp/log.do_populate_sdk.10545
ERROR: Task (/xxxx/AM62x/sdk/test/poky/meta-arago/meta-arago-distro/recipes-core/images/tisdk-default-image.bb:do_populate_sdk) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6803 tasks of which 6802 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 5 seconds
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 5 seconds
Summary: 1 task failed:
/xxxx/AM62x/sdk/test/poky/meta-arago/meta-arago-distro/recipes-core/images/tisdk-default-image.bb:do_populate_sdk
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
After adding the following to local.conf, the SDK can be generated.
RDEPENDS_packagegroup-core-standalone-sdk-target_remove = "libatomic-dev"
However when I installed the SDK, I got the following error and stuck there.
$ ./jome-2021.09-toolchain-2021.09.sh
Arago SDK installer version 2021.09
===================================
Enter target directory for SDK (default: /usr/local/jome-x86_64): /xxxx/AM62x/image-toolchain/20230131
You are about to install the SDK to "/xxxx/AM62x/image-toolchain/20230131". Proceed [Y/n]? Y
Extracting SDK............................................................................................................................................................................................................................................................................................................done
Setting it up...ls: cannot access '/xxxx/AM62x/image-toolchain/20230131/environment-setup-*': No such file or directory