Other Parts Discussed in Thread: AWR1843
I would like to drive the TM4C129ENCZAD on my custom board for the following purposes.
1. Convert USB signal to UART to communicate with other target.
2. Convert USB signals to JTAG signals to communicate with other ICs.
3. Display on the COM port when connected via USB. (Windows)
4. Drive as a USB device
Is it possible to create this by editing the program ourselves?
Also, which SDK for Tiva Ware should I refer to when making it?