Dear supporter,
In my newly developed device like the PROC105E8(001) have multiple power supplies from the PMIC(TPS65941515RWERQ1) to DRA821U4/LPDDR4.
Is the resistance of the power supply line a few ohms normal?
0.8V: VDD_CORE line: 3.8Ω
0.72V: VDD_CPU_AVS line: 23.5Ω
1.1V: VDD_DDR_1V1 line: 9.1Ω
0.85V: VDD_RAM_0V85 line: 106Ω
I'm worried that it will break when I turn on the power supply.