Other Parts Discussed in Thread: SYSCONFIG
Hi,
I followed this thread and tried to enable SPIDEV for SPI5 in SK-TDA4VM board.
I did the following,
1. Added SPI5 pins (Got the pins from SYSCONFIG) in k3-j721e-common-proc-board.dts file.
2. Added the SPIDEV node for main_spi5 in the k3-j721e-common-proc-board.dts file.
3. Made CONFIG_SPI_SPIDEV=y in tisdk_j7-evm_defconfig file.
4. Then ran the make command to build everything.
5. Then ran the following command to install the files to boot and rootfs of the SD card
host# sudo -E BOOTFS=/media/$USER/boot DESTDIR=/media/$USER/rootfs make install
6. Once the board is booted, checked the /dev folder not able to find the spidev in that.
7. As it was not working, I did the same thing in k3-j721e-sk-rpi-hdr-ehrpwm.dts file and again the result was the same.
Please suggest a solution for this.
Regards,
Surya